Arduino
  • Products
  • More
Arduino
Arduino Forum Simple circuiting question, using Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 30 replies
  • Answers 2 answers
  • Subscribers 420 subscribers
  • Views 3150 views
  • Users 0 members are here
Related

Simple circuiting question, using Arduino

e14 Contributor
e14 Contributor over 13 years ago

I want to control a 24v DC circuit with a my arduino, what would be the proper component and roughly how would I use it. Basically when I set a pin to high, I want it to switch the 24V on, and turn it off when set to low. From what I can gather, I need a MOSFET, but I have minimal knowledge on what to look for in one. Would someone be able to assist me?

 

(p.s. This is my first discussion, sorry if I am doing this incorrectly)

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 13 years ago in reply to ntewinkel +2
    Nico teWinkel wrote: You should probably at least have a resistor between the Arduino pin and the mosfet. [I've never designed with Arduino, so these are comments that apply to most microcontrollers.]…
  • ntewinkel
    ntewinkel over 13 years ago +1 suggested
    Hi Mason, You should probably at least have a resistor between the Arduino pin and the mosfet. Oomlout has a circuit example using a smaller transistor: http://www.oomlout.com/oom.php/products/ardx/circ…
  • ntewinkel
    ntewinkel over 13 years ago +1
    ps, this Instructable might also help: http://www.instructables.com/id/Use-Arduino-with-TIP120-transistor-to-control-moto/
Parents
  • ntewinkel
    0 ntewinkel over 13 years ago

    Hi Mason,

     

    You should probably at least have a resistor between the Arduino pin and the mosfet.

     

    Oomlout has a circuit example using a smaller transistor: http://www.oomlout.com/oom.php/products/ardx/circ-03

     

    Not sure if in your case you might also want an optocoupler (http://en.wikipedia.org/wiki/Opto-isolator) because of the difference in voltage.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 13 years ago in reply to ntewinkel

    Nico teWinkel wrote:

     

    You should probably at least have a resistor between the Arduino pin and the mosfet.

    [I've never designed with Arduino, so these are comments that apply to most microcontrollers.]

     

    I agree with this.  You need to protect the Arduino in the unlikely event that the NFET shorts between gate and source and presents 24V to the Arduino pin.  I would guess that the Arduino has internal clamping diodes to prevent pins from going too high, but those burn out at high currents.  So having a resistor (I usually start with 1K) controls the amount of current so that the clamp doesn't burn out.

     

    With an NFET, you also need to be concerned with what happens at power on.  Most micro-controllers boot with I/O pins floating, though some have weak pull-up or pull-down.  You'll probably want a pull-down resistor to ensure that your NFET is off when you first turn power on.  You don't need this with an NPN driver because the base-emitter junction will pull down if not driven high.

     

    If you're driving an inductive load like a motor, don't forget the flyback diode.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 13 years ago in reply to ntewinkel

    Nico teWinkel wrote:

     

    You should probably at least have a resistor between the Arduino pin and the mosfet.

    [I've never designed with Arduino, so these are comments that apply to most microcontrollers.]

     

    I agree with this.  You need to protect the Arduino in the unlikely event that the NFET shorts between gate and source and presents 24V to the Arduino pin.  I would guess that the Arduino has internal clamping diodes to prevent pins from going too high, but those burn out at high currents.  So having a resistor (I usually start with 1K) controls the amount of current so that the clamp doesn't burn out.

     

    With an NFET, you also need to be concerned with what happens at power on.  Most micro-controllers boot with I/O pins floating, though some have weak pull-up or pull-down.  You'll probably want a pull-down resistor to ensure that your NFET is off when you first turn power on.  You don't need this with an NPN driver because the base-emitter junction will pull down if not driven high.

     

    If you're driving an inductive load like a motor, don't forget the flyback diode.