Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Sketch Question?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 416 subscribers
  • Views 332 views
  • Users 0 members are here
  • i/o
  • push_buttons
  • sketch
  • multiple_buttons
  • digital_read
  • code
  • guitar_hero
  • ps3
  • array
  • arduino
  • question
Related

Arduino Sketch Question?

fechrxy
fechrxy over 13 years ago

So I am currently working on a project where I need to mod the five fret buttons of a ps3 guitar hero video game controller, I have already been sucesful in  individually hooking up the five buttons to the arduino's pins 5-10 and writing a sketch that can only one of the buttons. However I am not sure as to what is the best way to write the sketch so that it can read all five buttons. I need for example button 5, once pressed to be digitaly read and send a 1 to the serial monitor and button 6, once pressed to be digitaly read and send a 2 to the serial monitor ext. I believe I already know a few ways of doing this but they are somewhat indirect and don't seem the most efficent. I am sure if you have ever played guitar hero or any video game for that matter you can imagine the responce time that i would like to get with this, Thanks so much! 

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    0 mcb1 over 13 years ago

    Tony

    If you add Arduino to front of any google search, it envariably turns up lots of useful hits.

    In this case "arduino multiple buttons' gave 5,990,000 hits and this one looks like doing the work for you.

    http://www.adafruit.com/blog/2009/10/20/example-code-for-multi-button-checker-with-debouncing/

     

    You will always have issues with the speed to send data serially, so make sure the serial speed is as fast as it can be to reduce this time.

     

    You can also read ports which give a binary representation of each input, however to send it serially you need to process it, so there isn't a lot of gain.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 13 years ago

    Tony

    If you add Arduino to front of any google search, it envariably turns up lots of useful hits.

    In this case "arduino multiple buttons' gave 5,990,000 hits and this one looks like doing the work for you.

    http://www.adafruit.com/blog/2009/10/20/example-code-for-multi-button-checker-with-debouncing/

     

    You will always have issues with the speed to send data serially, so make sure the serial speed is as fast as it can be to reduce this time.

     

    You can also read ports which give a binary representation of each input, however to send it serially you need to process it, so there isn't a lot of gain.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer