Arduino
  • Products
  • More
Arduino
Arduino Forum Help me
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 15 replies
  • Subscribers 418 subscribers
  • Views 1878 views
  • Users 0 members are here
  • tutorial
  • help
  • prototyping
  • arduino
Related

Help me

tejaswivarma
tejaswivarma over 13 years ago

Hi,

          I am from india. I want to control the celing fan speed in my workshop (220V AC voltage) using arduino. can any one provide me with a circuit.

I need to control the speed by sending the data to arduino from my PC.

 

   thankyou in advance

 

                                                                      Have a nice day

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 13 years ago in reply to shabaz +1
    Shabaz You are quite right in that its complicated. Personally I would just go down to the local electrical store, and for a few dollars buy something that is approved and won't invalidate your insurance…
  • billabott
    billabott over 13 years ago +1
    For those interested in this topic; I think you may find this of interest: http://extremeelectronics.co.in/avr-projects/avr-project-remote-controlled-fan-regulator/ To purchase kit : http://store.extremeelectronics…
  • shabaz
    shabaz over 13 years ago in reply to billabott +1
    Hi Bill, You're better at google than me - that's actually not bad a circuit at the link you found, I couldn't find any! I can't see the PCB layout (so I'm not sure on the spacing between mains and low…
Parents
  • shabaz
    0 shabaz over 13 years ago

    Hi Indukuri,

     

    It's a very complicated topic. See this PDF document for some of the theory.

     

    In summary one traditional solution is to use a triac. Motors are inductive and are a challenge to confirm your circuit is good without test tools, becuase you won't know the inductance (it's not specified on fans). It could destroy your circuit. Your circuit may also have a lot of noise when it switches, unless you have zero-crossing detection. Also, it's highly likely that you could damage your PC or yourself, if you've not worked with such a circuit before.

     

    If you are curious to give it a go, be careful of circuits on the web, a lot of them are pretty ancient and don't have good practice.

     

    I don't know if this is good practice, but a more modern approach could be to make use of solid state relays (internally they use dual SCRs). I have some personal circuits for control of heaters but I don't plan to share them because I would worry if they had a fault. To give you a hint, I used a SSR and an external zero crossing detection circuit despite them having it built-in. I wouldn't know if that would meet a motor need, my heater element had a lower inductance than a motor. Another point is that inductive loads usually don't use zero-crossing SSRs, so that would be 'for further study' and experimentation by you. You may wish to move this question in one of the forums for SSRs, I think there is one for Crydom. It's not an Arduino related issue. Also, you may wish to change the title - 'Help me' is as you know not appropriate, it doesn't explain what the post is about.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to shabaz

    Shabaz

     

    You are quite right in that its complicated.

    Personally I would just go down to the local electrical store, and for a few dollars buy something that is approved and won't invalidate your insurance.

     

    I never give advice on playing with Mains, because I can't check the work prior to it being connected, and I've seen some potentially deadly lash-ups.

     

    The lighting fraternity used to use a 0-10v control system, and it may be possible to find some of these around.

    They are generally used when DMX control isn't.

     

    For ON/OFF control I highly recommend something that doesn't connect to a controller, and have used these previously.

    http://www.shop.wattsclever.com/11-usa-socket

    Some clever people have made a library to easily provide the sending end using a variety of devices so you have more than 3 devices available.

    http://code.google.com/p/rc-switch/

     

    mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 13 years ago in reply to shabaz

    Shabaz

     

    You are quite right in that its complicated.

    Personally I would just go down to the local electrical store, and for a few dollars buy something that is approved and won't invalidate your insurance.

     

    I never give advice on playing with Mains, because I can't check the work prior to it being connected, and I've seen some potentially deadly lash-ups.

     

    The lighting fraternity used to use a 0-10v control system, and it may be possible to find some of these around.

    They are generally used when DMX control isn't.

     

    For ON/OFF control I highly recommend something that doesn't connect to a controller, and have used these previously.

    http://www.shop.wattsclever.com/11-usa-socket

    Some clever people have made a library to easily provide the sending end using a variety of devices so you have more than 3 devices available.

    http://code.google.com/p/rc-switch/

     

    mark