Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino code help.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 1185 views
  • Users 0 members are here
  • buttons
  • led
  • code
  • arduino
Related

Arduino code help.

e14 Contributor
e14 Contributor over 12 years ago

I'm in the middle of an arduino project and I need help with the push buttons I'm using.

 

I need to be able to push a button that tells the arduino to set the LED value to 1 but not have the LED light up,

I also need there to be another button that makes all the push buttons that HAVE BEEN PRESSED light up.

 

Any help with the code or any resources that can help me are very much appreciated!

 

If this is not possible please tell me!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    The idea is to have a project box with about 10 buttons on the project box and little LEDs next to them, wherever the LEDs are placed, there will be pieces of paper indicating what each button represents…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Just explain me your project, I will try to help you. I can't understand what you really want  with your explanation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    The idea is to have a project box with about 10 buttons on the project box and little LEDs next to them, wherever the LEDs are placed, there will be pieces of paper indicating what each button represents next to the LEDs . The box would also have 2 buttons on the side of the project box, one would be used to turn on the leds that had their corresponding buttons pushed and the other

    would reset the system so it could be used with different combonations.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    That is a an easy code to program, you just have to set each push button to set a value "ON" on each correspondent LED.

     

    I don't understand what you want to do with the other two push buttons.

     

    I will not make the code for you since you are here to learn, so write your code and I will be glab to help you with any errors and give you any advise if you need.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • afmishaq
    0 afmishaq over 12 years ago in reply to e14 Contributor

    Hi Michael,

     

    You have an interesting project there. Did William Main's code solve your problem or you are still having difficulty?

     

    Faiz Ishaq

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to afmishaq

    I don't really understand the code sadly image

    I'm not that advanced with arduino programing yet,

    Could you possibly help me?

     

    Also

    Adding on extra chips seems hard, is there anything you could help me with to clear that up?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • afmishaq
    0 afmishaq over 12 years ago in reply to e14 Contributor

    You don't have to add any chips for now.

     

    I will write the sequence of things and then you can write the code yourself. I am sure you can write the code to light an LED on the press of a button.

     

    Let us start with a simle example of 4 buttons and 2 leds. The leds are led1 and led2. The buttons are btn1, btn2, btn-go and btn-rst.

     

    Normally, when btn1 is pressed you turn on led1. But here is what you want to do:

     

    - When btn1 is pressed you just mark that led1 will be turned on

    - When btn2 is pressed you just mark that led2 will be turned on

    - When the btn-go is pressed you turn on all the leds which have been marked to be turned on

    - When btn-rst is pressed you turn off all leds and set mark states to off

     

    You will need to define one memory variable to mark the state for each led, let us call them mrk1 and mrk2

     

    Now here is the code you have to write:

     

    to start with:

      mrk1=0

    mrk2=0

     

    on btn1 press:

      mrk1=1

     

    on btn2 press:

      mrk2=1

     

    on btn-go press:

      if mrk1=1, light led1

      if mrk2=1, light led2

     

    on btn-rst press:

      turn off led1

      turn off led2

      mrk1=0

      mrk2=0

     

    Hopefully, you can write and understand this code. Once you do it you will understand the other code, too. Just ask for more help if you have any problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to afmishaq

    Thanks so much for the help! I'm currently waiting on some more momentary switches so I won't be able to try out the code for a little while, but thanks for the

    help and if I need any more I'll be sure to ask you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to afmishaq

    Thanks so much for the help! I'm currently waiting on some more momentary switches so I won't be able to try out the code for a little while, but thanks for the

    help and if I need any more I'll be sure to ask you!