Arduino
  • Products
  • More
Arduino
Arduino Forum Hall effect flow meter help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 416 subscribers
  • Views 550 views
  • Users 0 members are here
Related

Hall effect flow meter help

e14 Contributor
e14 Contributor over 12 years ago

I have a hall effect flow meter and I can get it to read the current flow.....but, what I need to do is read the total  (say 100 litres) and then stop the flow thru a solenoid.  At the same time have a redundant timed stop that starts timing when the flow starts...energizing the solenoid, then de-energizing the solenoid (stopping flow) after 10 minutes.  I have no idea how to do the code here...please help.  Also, was wondering if I could done with Minibloq graffic programer? (or is minibloq limited)....as I'm using this for the rest of this project.  Thank you GJ.

  • Sign in to reply
  • Cancel

Top Replies

  • billpenner
    billpenner over 12 years ago in reply to e14 Contributor +1
    You will need to count the number of pulses in a period of time to calculate the total volume. The sensor specs. will have a factor specified which will indicate the liters/pulse. You will need a timer…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Am I clear on what I'm tryin' to do?  Basically I want to fill a tank to a specific volume....and then stop the filling.  Tho I'm very new to arduino I am amazingly able to read the flow rate thru the flow sensor...I just can't get a total in litres or whatever.  Am I overlooking something simple and obvious?

     

    Oh,....and is this the right place to post this?

     

    Thanks....GJ

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 12 years ago in reply to e14 Contributor

    Hi Jack,

     

    I'm no expert in this : ( but maybe a float switch would be easier to judge a specific level, rather than a flow sensor.

     

    However, if you are already able to obtain the flow rate (e.g. liters per sec) , you just need to multiply by time  - the arduino has a wait function, so you can wait a specific time, e.g. 500msec. If the flow is variable, you do the same thing, but technically an integration, which again you can do by multiplication (and summation) - also known as area under the curve - wikipedia on integration will have the info.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 12 years ago in reply to e14 Contributor

    Hi Jack,

     

    I'm no expert in this : ( but maybe a float switch would be easier to judge a specific level, rather than a flow sensor.

     

    However, if you are already able to obtain the flow rate (e.g. liters per sec) , you just need to multiply by time  - the arduino has a wait function, so you can wait a specific time, e.g. 500msec. If the flow is variable, you do the same thing, but technically an integration, which again you can do by multiplication (and summation) - also known as area under the curve - wikipedia on integration will have the info.