I have a hall effect flow meter and I can get it to read the current flow.....but, what I need to do is read the total (say 100 litres) and then stop the flow thru a solenoid. At the same time have a redundant timed stop that starts timing when the flow starts...energizing the solenoid, then de-energizing the solenoid (stopping flow) after 10 minutes. I have no idea how to do the code here...please help. Also, was wondering if I could done with Minibloq graffic programer? (or is minibloq limited)....as I'm using this for the rest of this project. Thank you GJ.