Arduino Forum Arduino resets when solenoid shuts off
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
  • State Suggested Answer
  • Replies 54 replies
  • Answers 16 answers
  • Subscribers 396 subscribers
  • Views 8630 views
  • Users 0 members are here
  • emi_protection
  • arduino
Related

Arduino resets when solenoid shuts off

Former Member
Former Member over 11 years ago

I have an arduino hooked to a 2 relay board. Each relay is opto-isolated. The arduino and board each have their own 5V power feed. The relays are switching 12V to controll a motor and a solenoid valve.

Sometimes when the solenoid turns off, the arduino resets. From what I've read, it's likely an EMI problem caused by the solenoid. If I disconnect the solenoid, I don't see the problem.

I've seen various suggestions about using a varistor or a diode, but I don't know which is better or what values to try. Any recommendations?

I'm assuming that the varistor or diode should be as close to the solenoid as possible, shorting the power and ground lines, is this correct?

 

Thanks,

Chris

  • Sign in to reply
  • Cancel

Top Replies

  • c4m4ch0
    c4m4ch0 over 8 years ago in reply to maranatha +3 suggested
    Hello maranatha, you just need to connect the diode as it is in this image
  • Former Member
    Former Member over 11 years ago in reply to michaelkellett +2 suggested
    I put an IN4004 Rectifier Diode across the terminals of the solenoid and that seems to have solved the problem. I also found this page pretty educational: http://en.wikipedia.org/wiki/Flyback_diode
  • maranatha
    maranatha over 8 years ago in reply to Former Member +1
    Hi Chris Do you happen to have the connection diagram? I am facing similar problem and it would be really helpful if you could share a connection diagram (basically how you connect the rectifier diode…
Parents
  • D_Hersey
    0 D_Hersey over 8 years ago

    You may also want to use some ferrite beads on your power feed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 8 years ago

    You may also want to use some ferrite beads on your power feed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • maranatha
    0 maranatha over 8 years ago in reply to D_Hersey

    Hi Don

     

    Where exactly to place the ferrite beads? For the arduino power feed or the raspberry pi power feed?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 8 years ago in reply to maranatha

    Why not both?  You should use a mix that is just a little slower than the signals you are trying to suppress

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 8 years ago in reply to D_Hersey

    Trying to find the root cause first.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to COMPACT

    In nearly every conversation we've had on this forum that involved a stepper, relay or other inductive load, adding a large (10,000uF) cap fixes it.

     

    Most people are not using a decent supply with suitable capacitance to handle the spike, and therfore when it is energised it causes a brownout on the supply which resets the Arduino.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 8 years ago in reply to mcb1

    Didn't I already suggest that as a possible cause by saying - "You also need enough power budget on the driving voltage as not cause it to sag and stop correct operation."

     

    It doesn't immediately explain why the lack of connection of an HDMI monitor to the Rpi is causing the arduino to misbehave.

    From what I understand thus far;

     

    • The arduino and Rpi work fine when the Rpi is connected or not connected to an HDMI monitor if the RPi and arduino are not connected together but can be in close proximity to each other.

     

    • The arduino becomes intermittently unstable when its relay is controlling the Rpi power only when no HDMI monitor is connected to the Rpi.

     

    However I don't know the behaviour when the Rpi Power is not controlled by the arduino but with only one Rpi power lead connected to the relay (with or without the HDMI monitor attached to the RPi).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • maranatha
    0 maranatha over 8 years ago in reply to COMPACT

    Hi COMPACT

     

    Yes, you did say "You also need enough power budget on the driving voltage as not cause it to sag and stop correct operation." My battery can provide 2.1A@5V for the RPi and I thought that should be fine. I also tried to power the Arduino from an external power supply 2.25A @7-12V.

     

    If I understand your last question correctly, I think I already answered what happens when one of the RPi power lead is connected to the relay (in the three points I mentioned before). The Arduino doesn't reset. I tried both power leads one by one and it didn't affect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 8 years ago in reply to maranatha

    So is the problem only evident when the Rpi power is switched on/off by the arduino relay?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • maranatha
    0 maranatha over 8 years ago in reply to COMPACT

    Yes, that is the situation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 8 years ago in reply to maranatha

    Is it only at the time the Rpi is turned on?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • maranatha
    0 maranatha over 8 years ago in reply to COMPACT

    The relay unlatches after few seconds (~3-4 sec)