Arduino
  • Products
  • More
Arduino
Arduino Forum weather sensor help!?!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 419 subscribers
  • Views 1662 views
  • Users 0 members are here
  • outdoor
  • humidity
  • weather
  • sensor
Related

weather sensor help!?!

funinalaska
funinalaska over 12 years ago

Does anyone know of a outdoor humidity sensor that works in extremely cold temps?

I need something that is moisture save and that will work at temperatures well below -40

I need it to have a minimum 2M watertight lead.

Right now for temperature I am using the DS18B20

It works for temperature but have now discovered I also need humidity readings as well.

  • Sign in to reply
  • Cancel
Parents
  • kas.lewis
    0 kas.lewis over 12 years ago


    I believe this from Measurement Specialists one can do -60, I know that may be just on the edge of acceptable for you but I will keep my eyes open for anything else that may be out there.

     

    Hope this helps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • funinalaska
    0 funinalaska over 12 years ago in reply to kas.lewis

    Well, the -60C it is rated for is a lot better than anything else I have run across.

    Now I get to research and see if I can find any Arduino libraries out there for it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kas.lewis
    0 kas.lewis over 12 years ago in reply to funinalaska

    Good luck with that, image

     

    If there is a library that will read a capacitance value then there is a function to turn that into a RH (%) {RH (%) = -3.4656 10+3*X3+1.0732 10+4*X2-1.0457 10+4*X+3.2459 10+3 With X=(C(read) / C@55%RH)}. I have not worked very much with Arduino but I did find this library and this example.

     

    Hope to hear how your project goes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kas.lewis
    0 kas.lewis over 12 years ago in reply to funinalaska

    Good luck with that, image

     

    If there is a library that will read a capacitance value then there is a function to turn that into a RH (%) {RH (%) = -3.4656 10+3*X3+1.0732 10+4*X2-1.0457 10+4*X+3.2459 10+3 With X=(C(read) / C@55%RH)}. I have not worked very much with Arduino but I did find this library and this example.

     

    Hope to hear how your project goes