Arduino
  • Products
  • More
Arduino
Arduino Forum weather sensor help!?!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 419 subscribers
  • Views 1660 views
  • Users 0 members are here
  • outdoor
  • humidity
  • weather
  • sensor
Related

weather sensor help!?!

funinalaska
funinalaska over 12 years ago

Does anyone know of a outdoor humidity sensor that works in extremely cold temps?

I need something that is moisture save and that will work at temperatures well below -40

I need it to have a minimum 2M watertight lead.

Right now for temperature I am using the DS18B20

It works for temperature but have now discovered I also need humidity readings as well.

  • Sign in to reply
  • Cancel
  • klong84
    0 klong84 over 12 years ago

    Hi, Sensirion makes several TEMP/HUMIDITY sensors from $6-$70 depending on the degree of resolution. Ebay carries many: the low end, DHT22 AM2302 Digital Temperature and Humidity Sensor Replace SHT10 SHT11 SHT15 | eBay for $5.58, rated for -40 - +125°C (-40 - +257°F). Just seek SHT[10,11,15,20,21,25,71,75] .

    Keith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • funinalaska
    0 funinalaska over 12 years ago in reply to klong84

    Yes, I am aware of the DHT22

    But as I said I need something that goes WELL BELOW -40

    I guess I should clarify, we regularly see temperatures below -50C

    and fairly common are temperatures below -55C

     

    Also since our temperature range here is fairly drastic

    -55C in winter up to about 25C in the summer, what is the best way to protect a sensor such as these outdoors from precipitation, blowing precipitation (snow) and dew?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kas.lewis
    0 kas.lewis over 12 years ago


    I believe this from Measurement Specialists one can do -60, I know that may be just on the edge of acceptable for you but I will keep my eyes open for anything else that may be out there.

     

    Hope this helps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • funinalaska
    0 funinalaska over 12 years ago in reply to kas.lewis

    Well, the -60C it is rated for is a lot better than anything else I have run across.

    Now I get to research and see if I can find any Arduino libraries out there for it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kas.lewis
    0 kas.lewis over 12 years ago in reply to funinalaska

    Good luck with that, image

     

    If there is a library that will read a capacitance value then there is a function to turn that into a RH (%) {RH (%) = -3.4656 10+3*X3+1.0732 10+4*X2-1.0457 10+4*X+3.2459 10+3 With X=(C(read) / C@55%RH)}. I have not worked very much with Arduino but I did find this library and this example.

     

    Hope to hear how your project goes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hope this helps finding a solution.

    .

    Just keep in mind that RH stand for relative humidity. If the water in the air (humidity) freeze the RH = 0% in any case. Thus the sensor must just survive the extreme cold condition while RH will be 0%.

      There is also a method of reading RH with a wet and dry temperature sensor if you find it difficult finding a RH sensor to survive the extreme cold condition. Formula for this calculation should be available on the net.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    O

    The last method mentioned (wet dry). I found more reliable and durable. The capacitive sensors tend to hold up better but need to be re-calibrated from time to time. I have done incubation controllers in the past and experience extreme pain on RH sensors. Land me eventually on the wet dry method.

      But in incubation: By controlling the temperature (dry reading) is held stable there for the RH control were not too difficult and controlled the RH with a fixed offset from “temperature reading (dry reading)” by using the wet reading.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kas.lewis
    0 kas.lewis over 12 years ago in reply to e14 Contributor

    bensmith can you provide a link to this method as it does sound interesting.

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • funinalaska
    0 funinalaska over 12 years ago

    I am beginning to think that I will just be better off figuring out how to access the airport's weather data. It is about 1/2 mile from me but their temperature readings are consistently 2 to 5 degrees F colder that readings I get here at my house. I blame it on the fact that the airport's weather station is a good 100 yards away from an structure or any form of wind or weather break. I have not yet figured out how to get my ethernet shield to do all the tasks I wish to ask from it, but it seems that sourcing their data from the METAR service will be much more reliable for humidity and wind speed than to implement my own sensors for those variables.

    We are getting to the time of year where the weather here is beginning to push the limits of some sensors and if this fall is any indication we could be in for a very wild ride this winter.

    Thank you all for the help and for the advise.

    I have many other questions but for now I will need to set aside this project for the holidays as I will be leaving this cold place for a still cold but not quite as harsh place at least for a few days.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kas.lewis
    0 kas.lewis over 12 years ago in reply to funinalaska

    If I may ask, how far north are you ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>