Arduino
  • Products
  • More
Arduino
Arduino Forum weather sensor help!?!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 419 subscribers
  • Views 1662 views
  • Users 0 members are here
  • outdoor
  • humidity
  • weather
  • sensor
Related

weather sensor help!?!

funinalaska
funinalaska over 12 years ago

Does anyone know of a outdoor humidity sensor that works in extremely cold temps?

I need something that is moisture save and that will work at temperatures well below -40

I need it to have a minimum 2M watertight lead.

Right now for temperature I am using the DS18B20

It works for temperature but have now discovered I also need humidity readings as well.

  • Sign in to reply
  • Cancel
Parents
  • klong84
    0 klong84 over 12 years ago

    Hi, Sensirion makes several TEMP/HUMIDITY sensors from $6-$70 depending on the degree of resolution. Ebay carries many: the low end, DHT22 AM2302 Digital Temperature and Humidity Sensor Replace SHT10 SHT11 SHT15 | eBay for $5.58, rated for -40 - +125°C (-40 - +257°F). Just seek SHT[10,11,15,20,21,25,71,75] .

    Keith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • klong84
    0 klong84 over 12 years ago

    Hi, Sensirion makes several TEMP/HUMIDITY sensors from $6-$70 depending on the degree of resolution. Ebay carries many: the low end, DHT22 AM2302 Digital Temperature and Humidity Sensor Replace SHT10 SHT11 SHT15 | eBay for $5.58, rated for -40 - +125°C (-40 - +257°F). Just seek SHT[10,11,15,20,21,25,71,75] .

    Keith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • funinalaska
    0 funinalaska over 12 years ago in reply to klong84

    Yes, I am aware of the DHT22

    But as I said I need something that goes WELL BELOW -40

    I guess I should clarify, we regularly see temperatures below -50C

    and fairly common are temperatures below -55C

     

    Also since our temperature range here is fairly drastic

    -55C in winter up to about 25C in the summer, what is the best way to protect a sensor such as these outdoors from precipitation, blowing precipitation (snow) and dew?