Arduino
  • Products
  • More
Arduino
Arduino Forum weather sensor help!?!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 419 subscribers
  • Views 1662 views
  • Users 0 members are here
  • outdoor
  • humidity
  • weather
  • sensor
Related

weather sensor help!?!

funinalaska
funinalaska over 12 years ago

Does anyone know of a outdoor humidity sensor that works in extremely cold temps?

I need something that is moisture save and that will work at temperatures well below -40

I need it to have a minimum 2M watertight lead.

Right now for temperature I am using the DS18B20

It works for temperature but have now discovered I also need humidity readings as well.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hope this helps finding a solution.

    .

    Just keep in mind that RH stand for relative humidity. If the water in the air (humidity) freeze the RH = 0% in any case. Thus the sensor must just survive the extreme cold condition while RH will be 0%.

      There is also a method of reading RH with a wet and dry temperature sensor if you find it difficult finding a RH sensor to survive the extreme cold condition. Formula for this calculation should be available on the net.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hope this helps finding a solution.

    .

    Just keep in mind that RH stand for relative humidity. If the water in the air (humidity) freeze the RH = 0% in any case. Thus the sensor must just survive the extreme cold condition while RH will be 0%.

      There is also a method of reading RH with a wet and dry temperature sensor if you find it difficult finding a RH sensor to survive the extreme cold condition. Formula for this calculation should be available on the net.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    O

    The last method mentioned (wet dry). I found more reliable and durable. The capacitive sensors tend to hold up better but need to be re-calibrated from time to time. I have done incubation controllers in the past and experience extreme pain on RH sensors. Land me eventually on the wet dry method.

      But in incubation: By controlling the temperature (dry reading) is held stable there for the RH control were not too difficult and controlled the RH with a fixed offset from “temperature reading (dry reading)” by using the wet reading.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kas.lewis
    0 kas.lewis over 12 years ago in reply to e14 Contributor

    bensmith can you provide a link to this method as it does sound interesting.

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to kas.lewis

    It has been some time ago that I have done Incubation using RH measurements (1995).

     

    Some links to explain what I were explaining.

    From Wikipedia Relative humidity - Wikipedia, the free encyclopedia.

    and Hygrometer - Wikipedia, the free encyclopedia . On this page the Wet Dry is explained. The "Hair tension hygrometers" on this page is most probable the one used at your airport.

    A technical doc http://www.vaisala.com/Vaisala%20Documents/Application%20notes/Humidity_Conversion_Formulas_B210973EN-F.pdf

    Above a bit too intensive for this discussion but any case it is there to read.

     

    To keep it simple. For a weather station use a simple curve fit formula to follow the chart at where the WS is situated to obtain the RH value from Wet/Dry. Psychrometrics - Wikipedia, the free encyclopedia

    Or just table the values in 5% or 10% increments and linear calculate the RH between 2 points will have an accuracy 2-3%RH (well suited for a WS +-5%RH)

    Keep in mind if you are in a 1%RH accuracy I deem it extremely accurate. For to find an instrument in less than 1%RH is very expensive and need to be calibrated with buffers before use every time.

     

    Else

    Look at SiLabs IC's Si7013/20/21 Humidity Sensors | Silicon Labs

    -40C to +125C operating.

    main page is Humidity and Temperature Sensor ICs | Silicon Labs

    I always had a good reliability experience from SiLabs components.