Arduino Forum I Want To Make My Own Arduino Uno Board Is There Any Way To Make One At Home ??
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
  • State Suggested Answer
  • Replies 16 replies
  • Answers 10 answers
  • Subscribers 398 subscribers
  • Views 1090 views
  • Users 0 members are here
  • board
  • own
  • uno
  • my
  • arduino
Related

I Want To Make My Own Arduino Uno Board Is There Any Way To Make One At Home ??

saurocksall
saurocksall over 11 years ago

hi to all, i want to make my own arduino uno board, is it possible to make one at home ?? i have a arduino uno r3 and have made many fun projects with it i wanted to know can i make one at home as is is open sourced it would not be that difficult to do, has any one here done that ??  would like some help ...

  • Sign in to reply
  • Cancel

Top Replies

  • Nate1616
    Nate1616 over 11 years ago +3 suggested
    Hey Saurabh There are many documents/websites out there that show how to make Arduinos. Here is just one doing a quick google search How to make your own Arduino board . I have also made this one that…
  • bwelsby
    bwelsby over 8 years ago +3 suggested
    Here's one way to build an arduino , http://make.kosakalab.com/make/obaka-project/aruduino-skeleton_en
  • ntewinkel
    ntewinkel over 11 years ago +2 suggested
    The good folks at Oomlout put together this nice Instructable that should make it very easy: How to Breadboard Arduino Compatible. I've seen other Arduino-on-a-breadboard type Instructables there too,…
Parents
  • balearicdynamics
    0 balearicdynamics over 9 years ago

    Hello Saurabh!

     

    As all the other user friends says, that answer is yes you can ! There are a couple of things that maybe useful for you in the specific case. I don't know what kind of projects you have in mind (maybe a good idea to share them with us ?); We assume that it is really super-easy to make your arduino board - IMHO the absolutely easier is just the Paperduino project creating an Arduino compatibile board on a piece of paper image

    Then maybe you make things more easier for your specific projects. Instead of making the general purpose Arduino board with the advantage to be able to recycle indefinitely the board you can make for less than the cost of the commercial Arduino your own dedicated Arduino-like boards. 100% compatible with Arduino you can integrate the base circuit of the microcontroller with your dedicated components excluding all those parts that are not useful for you. The result is that you can obtain a Arduino compatible board running on your project, something original just done by you.

     

    Here are some examples I have used in past:

     

    TiltPan Micro Camera is up and running !!!

    Microcontroller Health Status Controller Board based on AVR328p

     

    The following is the schemits of another Arduino dedicated board. I hope this suggestion maybe useful, if you need more information let me know.

    Enrico

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 9 years ago

    Hello Saurabh!

     

    As all the other user friends says, that answer is yes you can ! There are a couple of things that maybe useful for you in the specific case. I don't know what kind of projects you have in mind (maybe a good idea to share them with us ?); We assume that it is really super-easy to make your arduino board - IMHO the absolutely easier is just the Paperduino project creating an Arduino compatibile board on a piece of paper image

    Then maybe you make things more easier for your specific projects. Instead of making the general purpose Arduino board with the advantage to be able to recycle indefinitely the board you can make for less than the cost of the commercial Arduino your own dedicated Arduino-like boards. 100% compatible with Arduino you can integrate the base circuit of the microcontroller with your dedicated components excluding all those parts that are not useful for you. The result is that you can obtain a Arduino compatible board running on your project, something original just done by you.

     

    Here are some examples I have used in past:

     

    TiltPan Micro Camera is up and running !!!

    Microcontroller Health Status Controller Board based on AVR328p

     

    The following is the schemits of another Arduino dedicated board. I hope this suggestion maybe useful, if you need more information let me know.

    Enrico

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer