Arduino Forum I Want To Make My Own Arduino Uno Board Is There Any Way To Make One At Home ??
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
  • State Suggested Answer
  • Replies 16 replies
  • Answers 10 answers
  • Subscribers 398 subscribers
  • Views 1090 views
  • Users 0 members are here
  • board
  • own
  • uno
  • my
  • arduino
Related

I Want To Make My Own Arduino Uno Board Is There Any Way To Make One At Home ??

saurocksall
saurocksall over 11 years ago

hi to all, i want to make my own arduino uno board, is it possible to make one at home ?? i have a arduino uno r3 and have made many fun projects with it i wanted to know can i make one at home as is is open sourced it would not be that difficult to do, has any one here done that ??  would like some help ...

  • Sign in to reply
  • Cancel

Top Replies

  • Nate1616
    Nate1616 over 11 years ago +3 suggested
    Hey Saurabh There are many documents/websites out there that show how to make Arduinos. Here is just one doing a quick google search How to make your own Arduino board . I have also made this one that…
  • bwelsby
    bwelsby over 8 years ago +3 suggested
    Here's one way to build an arduino , http://make.kosakalab.com/make/obaka-project/aruduino-skeleton_en
  • ntewinkel
    ntewinkel over 11 years ago +2 suggested
    The good folks at Oomlout put together this nice Instructable that should make it very easy: How to Breadboard Arduino Compatible. I've seen other Arduino-on-a-breadboard type Instructables there too,…
Parents
  • ravi_butani
    0 ravi_butani over 8 years ago

    well u can even mk it on breadboard....what exactly you need here to mk ur own Arduino on breadboard is usb-uart converter and AtMega328 uC with arduino bootloader.... even Crystal is not compulsory...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 8 years ago in reply to ravi_butani

    Hi Ravi,

     

    Yoi mean that it can work without crystal too?  Sounds very strange to me!

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ravi_butani
    0 ravi_butani over 8 years ago in reply to balearicdynamics

    True Atmega Standalone, Running without crystal oscillator (Arduino) - All

     

    As AVR Atmega328 have internal selectable clock of 1,2,4,8MHz, its possible to use it with Arduino IDE without crystal... Only thing required is in Arduino IDE should Have board option with internal clock... board definations are available on above link...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 8 years ago in reply to ravi_butani

    Interesting, I have not considered this detail due the speed (or non-speed image) of the processor running at 8MHz but it is true, in theory it can do it.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 8 years ago in reply to ravi_butani

    Interesting, I have not considered this detail due the speed (or non-speed image) of the processor running at 8MHz but it is true, in theory it can do it.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • ravi_butani
    0 ravi_butani over 8 years ago in reply to balearicdynamics

    I am teaching AVR microcontroller subject in Master of engineering here in India... Not only Atmega328 (28-pin) even AtMega32(40-pin) AVR uC, we are using in lab with Arduino IDE and AVR Studio... and its on breadboard without crystal... and....Even no reset circuit is compulsory....

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to balearicdynamics

    There is also a 128kHz internal oscillator which can be used for low power applications.

    http://www.atmel.com/Images/Atmel-42735-8-bit-AVR-Microcontroller-ATmega328-328P_datasheet.pdf

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer