Arduino
  • Products
  • More
Arduino
Arduino Forum Toggle switch to push button switch conversion (Arduino or IC logic)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 62 replies
  • Answers 13 answers
  • Subscribers 422 subscribers
  • Views 10933 views
  • Users 0 members are here
  • push
  • toggle
  • trigger
  • button
  • flight
  • switch
  • arduino
  • simulator
Related

Toggle switch to push button switch conversion (Arduino or IC logic)

silviustro
silviustro over 12 years ago

     I would like to build an interface for a flight simulator consisting on various toggle and trigger switches, unfortunately i can't just simply flip a switch to an ON state and leave the signal like that, i need to send a quick pulse every time you toggle the switch ON or OFF, as if you where to push a button on a keyboard to send that command.

 

     In simple words... i need a toggle switch that will produce one pulse when you flip the toggle switch ON. And a second pulse will be generated when the same toggle switch is flipped to OFF. Here is a GIF to better illustrate that... http://www.desktopaviator.com/Products/Model_2120/2120B.gif

 

     If there is a simpler way of doing this without using an Arduino, like an IC or a special toggle swich, I would like to know, otherwise, I plan on using an Arduino to do this.

 

 

Thank you for your time!

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 12 years ago +3 suggested
    Hi Silviu, An easy method to produce pulses is to get a 'quad XOR gate' ic. Connecting one input of a gate to 0V makes a simple buffer which does nothing except delay a signal slightly. Do this with three…
  • shabaz
    shabaz over 12 years ago in reply to silviustro +2 suggested
    Hi Silviu, If you want to do it using an Arduino alone, you will need 80 pins for 40 switches and 40 outputs, so that may be unfeasible. Anyway, below is some pseudocode that will do it for (say) 4 switches…
  • jw0752
    jw0752 over 12 years ago in reply to silviustro +2 verified
    Hi Silviu; I have drawn a schematic and added some notes. . Don't worry about right answers as everyone contributes good ideas. If you have clarifying questions let me know. John
Parents
  • shabaz
    0 shabaz over 12 years ago

    Hi Silviu,

     

    An easy method to produce pulses is to get a 'quad XOR gate' ic.

     

    Connecting one input of a gate to 0V makes a simple buffer which does nothing except delay a signal slightly. Do this with three of the gates so that you have 3 buffers. Connect them up in series. Lets call them gates #1,2,3.

    Feed the final output from the third buffer (gate #3) into an input on the fourth gate. Connect your switch to 0V and (say) a 47k resistor to your supply rail. Connect the switch/resistor junction to the input of the fourth gate and the remaining input on gate#1.

     

    The end result is that you get a brief pulse (a few tens of nanosec) whenever the switch is opened or closed.

     

    But, I'm not sure this is what you really want. If (say) the power is off, and someone changes the toggle position and then powers on, then your software will have no idea what the initial toggle position is. Or, if the software is polling instead of using an interrupt, then it may skip some pulses (Maybe this is acceptable - depends on the actual application).

    For these reasons it would be best to try to design it so you can accept a normal toggle input, rather than a pulse if possible.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 12 years ago

    Hi Silviu,

     

    An easy method to produce pulses is to get a 'quad XOR gate' ic.

     

    Connecting one input of a gate to 0V makes a simple buffer which does nothing except delay a signal slightly. Do this with three of the gates so that you have 3 buffers. Connect them up in series. Lets call them gates #1,2,3.

    Feed the final output from the third buffer (gate #3) into an input on the fourth gate. Connect your switch to 0V and (say) a 47k resistor to your supply rail. Connect the switch/resistor junction to the input of the fourth gate and the remaining input on gate#1.

     

    The end result is that you get a brief pulse (a few tens of nanosec) whenever the switch is opened or closed.

     

    But, I'm not sure this is what you really want. If (say) the power is off, and someone changes the toggle position and then powers on, then your software will have no idea what the initial toggle position is. Or, if the software is polling instead of using an interrupt, then it may skip some pulses (Maybe this is acceptable - depends on the actual application).

    For these reasons it would be best to try to design it so you can accept a normal toggle input, rather than a pulse if possible.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • silviustro
    0 silviustro over 12 years ago in reply to shabaz

    Thank you for your answer Shabaz,

     

    I have to say, i did tough of using a logic gate to produce the signal, tho, when you have 40 toggles you need to wire, it becomes inefficient. A tenth of a nanosecond wouldn't be enough, i'd need something like a half second pulse to trigger the command correctly.

     

    Now, is there a way of doing this with an MCU? preferably an Arduino, (something like, if toggle on, then turn on led for one second, then if toggle off, do the same) I'd test it out with an LED, then replace it with an optocoupler. I have done the reverse, making a push button toggle a motor ON and OFF, but even then, i needed help with the code regarding the buffer of the Arduino. (i think using a delay without a loop would work, wouldn't it? the LED would turn on, and then stay off?)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 12 years ago in reply to silviustro

    Hi Silviu,

     

    If you want to do it using an Arduino alone, you will need 80 pins for 40 switches and 40 outputs, so that may be unfeasible.

    Anyway, below is some pseudocode that will do it for (say) 4 switches and 4 outputs. It is pseudocode since I'm not totally

    familiar with Arduino and won't compile, but it should give you ideas on how to arrange your code. It's not particularly efficient

    code, but was a quick thing. The logic should hopefully make sense, so that you can translate it into code.

     

    // assume inputs are numbered 0-3
    // assume outputs are numbered 4-7
    
    set_outputs_low()
    {
        // this function sets all four outputs low
        int k;
        for (k=4; k<8; k++)
        {
          digitalWrite(k, LOW);
        }
    }
    
    main()
    {
        int i;
        char newval;
        char togglestate[4];
       
         // set all outputs initially low
         set_outputs_low();
    
        // read the initial state of the 4 toggle switches connected to
        // inputs 0-3
        for (i=0; i<4; i++)
        {
          togglestate[i]=digitalRead[i];
        }
       
        while(1) // loop forever
        {
          // For all inputs, set an output high if a corresponding input has flipped
          for (i=0; i<4; i++)
            {
              newval=digitalRead[i];
              if (togglestate[i] <> newval) // has the state changed?
              {
                  togglestate[i]=newval;
                digitalWrite(i+4, HIGH); // set the corresponding output high
              }
            }
           
            // now sleep for half a second
            sleep(0.5);
           
            // now just set all outputs low
            set_outputs_low();
        } // loop forever
           
    }

     

    It sets an output high if it thinks the corresponding toggle input has changed from the previous value, and blindly sets all outputs low every half second, which has the desired end effect.

     

    If you want to scale to 40 inputs and 40 outputs with an Arduino then some form of I/O expansion is needed. This makes the circuit more complex and larger of course - things like PCF8574 can each handle 8 I/O, but there are surface mount devices that can do 16 I/O, or maybe higher.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • silviustro
    0 silviustro over 12 years ago in reply to shabaz

    Thank you very much Shabaz,

     

    I will sure check out and modify the code you gave, if usage of the Arduino I/O turns out too inefficient, i will research to find some kind of "special" momentary toggle switches, i know some old cars and planes use those kind of switches for ignition or other purposes. Thank you for your time, your answer was really helpful! (;

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 12 years ago in reply to silviustro

    I know this has been going around for the last 5 months or so but I thought I would throw my hat into the ring, as I have been working with Flight Simulators for a long, long time.... I have two basic questions:

    1. Which Flight Simulator is this for???
    2. Are you trying to simulate a keyboard?

    Most flight simulators use key mapping ie.. map a key to a function. I hope that is not what you are trying to do.. 

    Please see http://www.element14.com/community/people/phoenixcomm/blog/2013/05/30/nexgen-flight-simulator-hacking-the-navigation-computer-display

    Later ~~ Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 12 years ago in reply to shabaz

    Do not use this technique unless the logic family you are using publishes a minimum propagation delay!


    (NTBL)


    http://www.fairchildsemi.com/an/AN/AN-118.pdf

     

    RCA published an AN entitled 'CMOS multivibrators' or some-such which explains this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • smoot1
    0 smoot1 over 7 years ago in reply to shabaz

    I am in a technical rut maybe your method could help I need a sensor that when activated turns off a actuator and when released sends signal to reactivate actuator I'm not quite sure how I could make this possible sense I need sensor to be the size of a finger tip for instance

    senser is off actuator is fully extended locked sensor is activated by touch hold actuator releases and able to be pushed down manually and when sensor is released it activates sensor if you or anyone could shoot a response back to me be super appreciated and who ever helps me put with this hurdle and it works I will give royalties on my invention once patents are secured.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 7 years ago in reply to smoot1

    Shayne first let me figure out what you really need to do. I have been build sims for more than a few years. First, your two links are BUSTED. Second do have an interface spec of what you are trying to interface. (As most sim parts require levels) So I have some questions. what do you mean by "need a sensor that when activated turns off an actuator and when released sends a signal to reactivate actuator" and then you go on to say "I need a sensor to be the size of a fingertip for instance:

    • the sensor is off actuator is fully extended locked
    • the sensor is activated by touch hold actuator releases and able to be pushed down manually
    • and when the sensor is released it activates a sensor".

    You seem to be confused about what the components are or their names.

    This is what I think you want by taking the three lines apart

    1. the Switch is OFF when it is fully extended.
    2. When the Switch is pushed in and then releases (goes back to state 1) you send a signal (pulse) and the cycle starts again.

    To me, if I got this right it sounds like you are wanting to use some sort of keyboard.

    What function are you trying to turn off and on? which sim is this MS/X-plane/etc.

    If you referring to a switch like the one in your first post as the sensor? Then what is an actuator?? If you don't know I can't help (don't read minds). Are you trying to use (simulate) a keyboard??

    Have you looked at my blog posts?  just search for NexGen Blog index

    Cris.