Arduino Forum Arduino relays for lighting
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
  • State Suggested Answer
  • Replies 17 replies
  • Answers 3 answers
  • Subscribers 405 subscribers
  • Views 2517 views
  • Users 0 members are here
  • lighting
  • relays
  • arduino
Related

Arduino relays for lighting

Former Member
Former Member over 11 years ago

All,

 

I'm building a new house, and I decided that I want microcontrollers to control my lighting. Now I have dimmers covered, with a 0-+10V system, but surprisingly I'm struggling a bit with the lights that should just be on or off. I figured it should be doable with a relatively cheap array of relays connected to an Arduino. I'm not going to get my hands dirty, my electrician is (which is, I should say, a good idea). He insists on the following standard for the relays:

  • CE certification.
  • at least 240 VAC
  • at least 10A
  • DIN Rail mountable

 

I'm guessing I could satisfy the last requirement with a PCB in something like this: http://cpc.farnell.com/pulse/acc-case-m/flightcase-universal-medium/dp/DP31699

I have not yet found a product, that matches all of the top three though: I found something in various shops that has 250 VAC @ 10A, but no visible CE mark, and I found one on hobbyking http://hobbyking.com/hobbyking/store/__26921__Arduino_6_Channel_Relay_Module.html that had a CE mark, but could only do 240VAC @ 7A. I'd like something like that, with 6-8 channels would be nice.

 

It would be nice if the electrician could order all the products from Farnell, since they have a Norwegian office and I have used them for some other projects. Any pointers?

 

Message was edited by: Matt Collinge. Updated CPC link.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 9 years ago +2
    Your electrician is right in terms of good practice and it may well be that local laws require the parts to comply with his suggestions. I expect you would like your house to last at least 25 years before…
  • beacon_dave
    beacon_dave over 9 years ago in reply to michaelkellett +2 suggested
    Michael Kellett wrote: ...Arduino isn't the right kind of thing for this - I think you should go for industrial standard parts and practice which would suggest 24V DC relay coils... There are these Arduino…
  • shabaz
    shabaz over 9 years ago in reply to mcb1 +2
    There are even more possibilities, like activation without taking the device out the package : ) (I've no idea if Peter's device does that, but technically it is feasible). NXP has a part which can be…
Parents
  • mcb1
    0 mcb1 over 9 years ago

    michaelkellett is quite right about seperating the mains from the control side.

    We have discussed electrical safety before on the site and there are no shortcuts.

     

    The basic idea is to ensure that the low voltage control side and the mains are properly seperated.

    The relay unit you have does at least have the board cut to increase the seperation distance where the relays moutn to the board, however I'm not sure if the pcb track sizes are up to the 10A rating.

    On some versions the size is quite small and doesn't include a reinforcement wire to improve it.

     

    We talked it about safety and the importance of the insulation and physical distance during the Forget Me Not challenge.

    Forget Me Not :  eLDERmon  Electrical

     

    I suggested these since they are available to suit whatever mains outlet configuration the country has, and can be controlled by 433MHz RF.

    Forget Me Not :  eLDERmon  Outlets

     

    Since then there is another cheaper WiFi and RF solution and they even have one that interfaces between the light socket and a lamp.

    I believe someone has broken the coding to allow it to be used locally rather than their web server.

    Sonoff Smart Home Solution - ITEAD Wiki

     

     

    In short there are options but without the necessary approvals and safety inspections you could be creating a problem if there was an electrical event.

    Whether that is an accidental contact or the worst a fire, there may be questions raised and possible insurance issues.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 9 years ago

    michaelkellett is quite right about seperating the mains from the control side.

    We have discussed electrical safety before on the site and there are no shortcuts.

     

    The basic idea is to ensure that the low voltage control side and the mains are properly seperated.

    The relay unit you have does at least have the board cut to increase the seperation distance where the relays moutn to the board, however I'm not sure if the pcb track sizes are up to the 10A rating.

    On some versions the size is quite small and doesn't include a reinforcement wire to improve it.

     

    We talked it about safety and the importance of the insulation and physical distance during the Forget Me Not challenge.

    Forget Me Not :  eLDERmon  Electrical

     

    I suggested these since they are available to suit whatever mains outlet configuration the country has, and can be controlled by 433MHz RF.

    Forget Me Not :  eLDERmon  Outlets

     

    Since then there is another cheaper WiFi and RF solution and they even have one that interfaces between the light socket and a lamp.

    I believe someone has broken the coding to allow it to be used locally rather than their web server.

    Sonoff Smart Home Solution - ITEAD Wiki

     

     

    In short there are options but without the necessary approvals and safety inspections you could be creating a problem if there was an electrical event.

    Whether that is an accidental contact or the worst a fire, there may be questions raised and possible insurance issues.

     

    Mark