Arduino
  • Products
  • More
Arduino
Arduino Forum My Nokia LCD 5110 isn't work (just blue screen from backlight)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 21 replies
  • Subscribers 419 subscribers
  • Views 7215 views
  • Users 0 members are here
  • arduino
Related

My Nokia LCD 5110 isn't work (just blue screen from backlight)

e14 Contributor
e14 Contributor over 12 years ago

Hello everyone, I'm new in arduino, and i have a project by using nokia lcd 5110 and i bought it yesterday. But when i connect it with my arduino like in this tutorial https://learn.sparkfun.com/tutorials/graphic-lcd-hookup-guide/hardware-assembly--hookup , the backlight is on but the screen is blank(nothing show up in there just a blue color from backlight).         So can you please help me to solve this problem?image

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to saurocksall +1
    Ok, these are the pictures, can you please help me?
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to mcb1 +1
    Thanks for the tip! there is now a 330 ohm resistor in series with the BL(led) pin. I got this to work in the end by tweaking the bias and contrast settings on the lcd this tutorial: https://www.youtube…
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi everyone,

     

    - There are 6 resistors in the picture. Could anyone pls explain their part in the circuit? My displays (20) have flicker streaks across the screen. I wonder if i can do anything with circuit to make it clearly.     

    - I have the same display as in this post, which have build in level shifter to use with either 3,3V or 5V. It is powered by LM 7805 CV. I catch the same problem when other parts on my circuit draw too much from the power source. So i think you should try turn of the LEDs to save about 80mA.

     

    Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi everyone,

     

    - There are 6 resistors in the picture. Could anyone pls explain their part in the circuit? My displays (20) have flicker streaks across the screen. I wonder if i can do anything with circuit to make it clearly.     

    - I have the same display as in this post, which have build in level shifter to use with either 3,3V or 5V. It is powered by LM 7805 CV. I catch the same problem when other parts on my circuit draw too much from the power source. So i think you should try turn of the LEDs to save about 80mA.

     

    Thank you.