Arduino
  • Products
  • More
Arduino
Arduino Forum My Nokia LCD 5110 isn't work (just blue screen from backlight)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 21 replies
  • Subscribers 419 subscribers
  • Views 7175 views
  • Users 0 members are here
  • arduino
Related

My Nokia LCD 5110 isn't work (just blue screen from backlight)

e14 Contributor
e14 Contributor over 12 years ago

Hello everyone, I'm new in arduino, and i have a project by using nokia lcd 5110 and i bought it yesterday. But when i connect it with my arduino like in this tutorial https://learn.sparkfun.com/tutorials/graphic-lcd-hookup-guide/hardware-assembly--hookup , the backlight is on but the screen is blank(nothing show up in there just a blue color from backlight).         So can you please help me to solve this problem?image

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to saurocksall +1
    Ok, these are the pictures, can you please help me?
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to mcb1 +1
    Thanks for the tip! there is now a 330 ohm resistor in series with the BL(led) pin. I got this to work in the end by tweaking the bias and contrast settings on the lcd this tutorial: https://www.youtube…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    actually i have changed the configuration but the lcd still same like that. And because of that i confused with this. And i want to ask, do i have to use level shifter ic for this lcd? or replace the level shifter ic with resistor?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelwylie
    0 michaelwylie over 12 years ago in reply to e14 Contributor

    According to this link the basic Arduino is 5V and the display is 3V, so the level shifter is recommended. From your link:

    "The easiest hookup is to connect the Arduino pins directly to the LCD. To allow for this easy hookup, you’ll need a 3.3V-operating Arduino like the 3.3V/8MHz Pro or 3.3V Pro Mini." I think I'd try the resistors first, since they're likely more handy than the level shifter. I would also check the continuity of those wires.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelwylie
    0 michaelwylie over 12 years ago in reply to e14 Contributor

    According to this link the basic Arduino is 5V and the display is 3V, so the level shifter is recommended. From your link:

    "The easiest hookup is to connect the Arduino pins directly to the LCD. To allow for this easy hookup, you’ll need a 3.3V-operating Arduino like the 3.3V/8MHz Pro or 3.3V Pro Mini." I think I'd try the resistors first, since they're likely more handy than the level shifter. I would also check the continuity of those wires.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to michaelwylie

    Ok, i'll try your advise, thank you sir ! image