Arduino
  • Products
  • More
Arduino
Arduino Forum Hi im newbie and need help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 15 replies
  • Subscribers 418 subscribers
  • Views 1539 views
  • Users 0 members are here
Related

Hi im newbie and need help

e14 Contributor
e14 Contributor over 12 years ago

Does somebody can help me connect this driver to arduino unowww.escapmotor.com/MYCOM/pdf/2_phase_stepper/ims200.pdf.....im trying drive 6 wire stepper motor using it and didnt know it wiring connection....here i attach it datasheet

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to gihu +1
    thanks gihu.........now i wonder why the motor wont work. i try this simple arduino code and connected it but its not functioning. so if the library for the arduino is not suppport how can i drive this…
Parents
  • gihu
    0 gihu over 12 years ago

    Hi zamir,

     

    You can connect it has shown in point 5 (connection diagram), CW+ and CCW+ connected t 5V of the arduino, and CW- and CCW- connected to two different digital outputs of the arduino. But take into account that for this driver, the stepper library for arduino will not work.

     

    If you need more help with on how to program the arduino to move your stepper motor with this driver, ask.

     

    By the way, how will you connect the driver with the stepper?

     

    Regards,

    Miguel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to gihu

    thanks gihu.........now i wonder why the motor wont work. i try this simple arduino code and connected it but its not functioning. so if the library for the arduino is not suppport how can i drive this driver ?gihuimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    // define the pins that the motor is attached to. You can use

    // any digital I/O pins.

     

     

    #include <Stepper.h>

     

     

    #define motorSteps 200     // change this depending on the number of steps

                               // per revolution of your motor

    #define motorPin1 8

    #define motorPin2 9

    #define ledPin 13

     

     

    // initialize of the Stepper library:

    Stepper myStepper(motorSteps, motorPin1,motorPin2);

     

     

    void setup() {

      // set the motor speed at 60 RPMS:

      myStepper.setSpeed(60);

     

     

      // Initialize the Serial port:

      Serial.begin(9600);

     

     

      // set up the LED pin:

      pinMode(ledPin, OUTPUT);

      // blink the LED:

      blink(3);

    }

     

     

    void loop() {

      // Step forward 100 steps:

      Serial.println("Forward");

      myStepper.step(100);

      delay(500);

     

     

      // Step backward 100 steps:

      Serial.println("Backward");

      myStepper.step(-100);

      delay(500);

     

     

    }

     

     

    // Blink the reset LED:

    void blink(int howManyTimes) {

      int i;

      for (i=0; i< howManyTimes; i++) {

        digitalWrite(ledPin, HIGH);

        delay(200);

        digitalWrite(ledPin, LOW);

        delay(200);

      }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gihu
    0 gihu over 12 years ago in reply to e14 Contributor

    You sholud drive pulses directly to the digital outputs

     

    Try this, not using the library.

    Check that the jumpers in your driver are like this:

    JP1: 1-2

    JP2: 1-2

     

    code (I could not check errors):

    // define the pins that the motor is attached to. You can use

    // any digital I/O pins.

    //#include <Stepper.h>

    #define motorSteps 200 // change this depending on the number of steps

    // per revolution of your motor

    #define CW 8

    #define CCW 9

    #define ledPin 13

    // initialize of the Stepper library:

    //Stepper myStepper(motorSteps, motorPin1,motorPin2);

     

    void setup() {

    // set the motor speed at 60 RPMS:

    //myStepper.setSpeed(60);

      

     

    int i =0;

     

    // Initialize the Serial port:

     

    Serial.begin(9600);

     

    // set up the LED pin:

    pinMode(ledPin, OUTPUT);

    pinMode(CW, OUTPUT);

    pinMode(CCW, OUTPUT);

     

    // blink the LED:

     

    blink(3);

    digitalWrite(CW, HIGH);

    digitalWrite(CCW, HIGH);

    }

     

    void loop() {

     

    // Step forward 100 steps:

    Serial.println("Forward");

    //myStepper.step(100);

    for (i=0; i<100; i++){

    digitalWrite(CW, LOW);

    delayMicroseconds(20);

    digitalWrite(CW, HIGH);

    delayMicroseconds(20);

    };

    delay(500);

    // Step backward 100 steps:

    Serial.println("Backward");

    //myStepper.step(-100);

    for (i=0; i<100; i++){

    digitalWrite(CCW, LOW);

    delayMicroseconds(20);

    digitalWrite(CCW, HIGH);

    delayMicroseconds(20);

    };

    delay(500);

    }

     

    // Blink the reset LED:

    void blink(int howManyTimes) {

    int i;

    for (i=0; i< howManyTimes; i++) {

    digitalWrite(ledPin, HIGH);

    delay(200);

    digitalWrite(ledPin, LOW);

    delay(200);

    }

     

    }

     

     

    If it works, we can try to create a new library for your driver from the original Stepper lib.

     

    Regards,

    Miguel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to gihu

    hurmm i connected and use your instruction correctly but the motor still wont move

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gihu
    0 gihu over 12 years ago in reply to e14 Contributor

    Can you check if you have pulses in the digital outputs 8 and 9?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gihu
    0 gihu over 12 years ago in reply to e14 Contributor

    It seems someone else worked on this.

    Check this library for arduino:

    https://github.com/ronivaldo/Arduino-StepperMSeries

    But it seems to work for pulse/direction mode, not CW/CCW mode, so if you use it don't forget change hardware configuration

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to gihu

    owh thank you very much friends....i check on it...actually im thinking to

    make homemade cnc machine..:)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to gihu

    one more question....my driver doesnt have ground pin for arduino is it

    necessary?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to gihu

    i put an led and it blink....is that mean it got a pulse... i think maybe

    my stepper motor. here i sent it datasheet

    Attachments:
    imageAPPENDIX B.docx
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to gihu

    this is the 24v power supply i used

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to gihu

    this is the 24v power supply i used

    Attachments: