Arduino
  • Products
  • More
Arduino
Arduino Forum How can I power the Arduino Board or Raspberry Pi Board without connecting it to a computer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 418 subscribers
  • Views 901 views
  • Users 0 members are here
Related

How can I power the Arduino Board or Raspberry Pi Board without connecting it to a computer

the_future
the_future over 12 years ago

Hi

 

My name is Orlando and please forgive me if this seems like a stupid question but

I am only a beginner. This question i have came from an idea that if I had made a robot

i would not want it to always be connect to a computer, because it would limit movement.

So how can i power my robot or project without it always being connected to a computer while

still containing the code.

 

I am not sure but i think when code is uploaded to a board it permanent stays they till over wise

but I am not 100% sure

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    These are two examples of battery packs, the second will power any 5v unit you need and for quite some time, there are many others but this will get you started with all these things, its about perspective…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    I assume then you also need to be disconnected from a wall adapter for the same reason ?

     

    if so then a simple rechargeable battery pack would do the trick, the Arduino's do not have a tight power requirement like the TI Launch pads and you can feed them with a range of input from 5-12 or more volts

     

    if you check on Element 14 web site or Adafruit you will find battery packs for the Arduinos (Google "Battery Pack for Arduino" )

     

    hope this helps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    I assume then you also need to be disconnected from a wall adapter for the same reason ?

     

    if so then a simple rechargeable battery pack would do the trick, the Arduino's do not have a tight power requirement like the TI Launch pads and you can feed them with a range of input from 5-12 or more volts

     

    if you check on Element 14 web site or Adafruit you will find battery packs for the Arduinos (Google "Battery Pack for Arduino" )

     

    hope this helps