Arduino
  • Products
  • More
Arduino
Arduino Forum How can I power the Arduino Board or Raspberry Pi Board without connecting it to a computer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 418 subscribers
  • Views 903 views
  • Users 0 members are here
Related

How can I power the Arduino Board or Raspberry Pi Board without connecting it to a computer

the_future
the_future over 12 years ago

Hi

 

My name is Orlando and please forgive me if this seems like a stupid question but

I am only a beginner. This question i have came from an idea that if I had made a robot

i would not want it to always be connect to a computer, because it would limit movement.

So how can i power my robot or project without it always being connected to a computer while

still containing the code.

 

I am not sure but i think when code is uploaded to a board it permanent stays they till over wise

but I am not 100% sure

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    These are two examples of battery packs, the second will power any 5v unit you need and for quite some time, there are many others but this will get you started with all these things, its about perspective…
Parents
  • johnbeetem
    0 johnbeetem over 12 years ago

    Future Orlando wrote:

     

    I am not sure but i think when code is uploaded to a board it permanent stays they till over wise

    but I am not 100% sure

    Raspberry Pi stores all its software on the SD card, which is non-volatile storage and stores programs and data while power is off.  If you're running a Linux-based OS, before you power down or reset you usually need to give a "shutdown" or at least a "sync" command so that RAM buffers are written to the SD card, otherwise you could leave it the file system in a corrupted state.

     

    RasPi uses a lot more power than an Arduino, especially a Model B.  The Model A uses less power since it doesn't have the USB/Ethernet chip.

     

    Search for "battery operated Raspberry Pi" in the search box at the top of the page for how various people have powered RasPi using batteries.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 12 years ago

    Future Orlando wrote:

     

    I am not sure but i think when code is uploaded to a board it permanent stays they till over wise

    but I am not 100% sure

    Raspberry Pi stores all its software on the SD card, which is non-volatile storage and stores programs and data while power is off.  If you're running a Linux-based OS, before you power down or reset you usually need to give a "shutdown" or at least a "sync" command so that RAM buffers are written to the SD card, otherwise you could leave it the file system in a corrupted state.

     

    RasPi uses a lot more power than an Arduino, especially a Model B.  The Model A uses less power since it doesn't have the USB/Ethernet chip.

     

    Search for "battery operated Raspberry Pi" in the search box at the top of the page for how various people have powered RasPi using batteries.