Arduino
  • Products
  • More
Arduino
Arduino Forum RGB LED source or workaround
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 416 subscribers
  • Views 231 views
  • Users 0 members are here
  • common
  • cathod
  • rgb
  • for
  • source
  • led?
Related

RGB LED source or workaround

nrgymyzr
nrgymyzr over 12 years ago

In Jeremy's lesson 2 with the RGB, I was forced to go and purchase an RGB Led from Radio Shack.  I bought #276-008. The problem is that it has a common anode instead of a common cathode. They didn't appear to offer the kind your lesson was requiring.  Is there a wok around or better yet, a source to purchase it?

  • Sign in to reply
  • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    The only difference is that the common voltage for all the LEDs is + instead of -

     

    what that means to your code is instead of outputting a one (HIGH) to turn on the LED, you will output a zero (LOW). and the common pin of the LED will go to +5V instead of 0V

    instead of image

    Fullscreen 2376.contentimage_182503.html Download
    <html><head><title>Jive SBS</title></head>
    <body><font face="arial,helvetica,sans-serif">
    <b>Error</b><br><font size="-1">
    An general error occurred while processing your request.
    </font></font></body></html>
    

     

    So the significant difference is sending out a LOW to turn on the LED when the common of the LED is HIGH (Common Anode), and sending out a HIGH to turn on the LED when the common is LOW (Common Cathode)

    image

     

    So with very little modification you can adapt the program and simply move the common pin to 5 V instead of 0V. no need to go buy more LEDs

     

    Hope that answers your question