Arduino
  • Products
  • More
Arduino
Arduino Forum Need to learn how to code hour meter.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 3784 views
  • Users 0 members are here
  • meters
  • help
  • hour
  • arduino
Related

Need to learn how to code hour meter.

e14 Contributor
e14 Contributor over 12 years ago

Hello,

     I am new to Arduino and I am having a hard time figuring out how to create a hour meter. I am using an uno with an Ethernet/SD shield. I have that hooked up to sump pump and a transducer. I am able to see the liquid level and control the pump via web page. However, I would like to create a hour meter that records the pump run-time hours, and prints it on to the web page. Here is my code,

 

#include <SPI.h>
#include <Ethernet.h>

// Enter a MAC address and IP address for your controller below.
// The IP address will be dependent on your local network:
byte mac[] = {
  0xDE, 0xAD, 0xBE, 0xEF, 0xFE, 0xED };
IPAddress ip(192,168,1,177);

// Initialize the Ethernet server library
// with the IP address and port you want to use
// (port 80 is default for HTTP):
EthernetServer server(80);
*/ LEDpin is used to control relay
int LEDpin = 1;
String readString = String(30);
String state = String(3);

void setup()
{
  // start the Ethernet connection and the server:
  Ethernet.begin(mac, ip);
  server.begin();
 
  //Sets the LEDpin as an output
  //LEDpin is actually for relay control
  pinMode(LEDpin,OUTPUT);
 
  digitalWrite(LEDpin,LOW);
  state = "OFF";
}

void loop()
{
  // listen for incoming clients
  EthernetClient client = server.available();
  if (client) {
    // an http request ends with a blank line
    boolean currentLineIsBlank = true;
    while (client.connected()) {
      if (client.available()) {
        char c = client.read();
        // if you've gotten to the end of the line (received a newline
        // character) and the line is blank, the http request has ended,
        // so you can send a reply

        if (readString.length() < 30) {
          readString.concat(c);
        }

        if (c == '\n' && currentLineIsBlank) {
          // send a standard http response header
          int LED = readString.indexOf("LED=");

          if (readString.substring(LED,LED+5) == "LED=T") {
            digitalWrite(LEDpin,HIGH);
            state = "ON";
          }
          else if (readString.substring(LED,LED+5) == "LED=F") {
            digitalWrite(LEDpin,LOW);
            state = "OFF";
          }
          client.println("HTTP/1.1 200 OK");
          client.println("Content-Type: text/html");
          client.println("Connection: close");  // the connection will be closed after completion of the response
   client.println("Refresh: 3");  // refresh the page automatically every 3 sec
        
          client.println();

  client.println("<!DOCTYPE HTML>");
          client.println("<html><body bgcolor='Gray'>");
          // Pump Name
          client.println("<center><H1>KO6</H1></center>");
          // output the value of the analog input pin
          for (int analogChannel = 0; analogChannel < 1; analogChannel++) {
            int sensorReading = analogRead(analogChannel);
            sensorReading = map(sensorReading, 0, 1024, 0, 300);
            client.print("<center> Liquid Level ");
            client.print(" is ");
            client.print ("<b><font color='blue'>");
            client.print(sensorReading);
            client.print ("</b></font color>");
            client.println("<br />");
            client.print(" Hours:  ");
            //client.print(runtime)
            client.println("<br />");     
          }
        
         
          client.print("Pump is ");
          client.print(state);
          client.print("<br><br>");
         
          if (state == "ON") {
            client.println("<a href=\"./?LED=F\">Turn Off<a>");
          }
          else {
            client.println("<a href=\"./?LED=T\">Turn On<a>");
          }
           client.print("</center>");
           client.println("</html>");
          break;
        }
        if (c == '\n') {
          // you're starting a new line
          currentLineIsBlank = true;
        }
        else if (c != '\r') {
          // you've gotten a character on the current line
          currentLineIsBlank = false;
        }
      }
    }
    // give the web browser time to receive the data
    delay(1);
    readString = "";
    // close the connection:
    client.stop();
  }

 

Sorry if my code is sloppy, I am still learning, if anyone could help me it would be greatly appreciated.

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Are you looking to run a cumulative counter, or just keep track of the time that the pump runs in one "session"?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    jbix,

    I am looking to run a cumulative hour meter.

    I have modified my code below. but I am still having problems. all that I am getting is 0 for the hour reading.

    Not sure what I am doing wrong.

     

     

     

     

    [code]
    #include <SPI.h>
    #include <Ethernet.h>

    // Enter a MAC address and IP address for your controller below.
    // The IP address will be dependent on your local network:
    byte mac[] = {
      0xDE, 0xAD, 0xBE, 0xEF, 0xFE, 0xED };
    IPAddress ip(192,168,1,177);

    // Initialize the Ethernet server library
    // with the IP address and port you want to use
    // (port 80 is default for HTTP):
    EthernetServer server(80);
    // LEDpin is used to control relay
      int LEDpin = 1;
        //Declarations for the hour meter
        int startTime = millis();
        int stopTime = millis();
        int runTime =((stopTime) - (startTime))/1000;
        int onTime =+ runTime;

          String readString = String(30);
          String state = String(3);

    void setup()
    {
      // start the Ethernet connection and the server:
      Ethernet.begin(mac, ip);
      server.begin();
     
        //Sets the LEDpin as an output
        //LEDpin is actually for relay control
        pinMode(LEDpin,OUTPUT);
        //Sets the STATUSpin as an input
        //STATUSpin reads a signal to tell whether the pump is on or off


          //reset the pump state
          digitalWrite(LEDpin,LOW);
          state = "OFF";

    }

    void loop()

    {
        
      // listen for incoming clients
      EthernetClient client = server.available();
      if (client) {
        // an http request ends with a blank line
        boolean currentLineIsBlank = true;
        while (client.connected()) {
          if (client.available()) {
            char c = client.read();
            // if you've gotten to the end of the line (received a newline
            // character) and the line is blank, the http request has ended,
            // so you can send a reply

            if (readString.length() < 30) {
              readString.concat(c);
            }

            if (c == '\n' && currentLineIsBlank) {
              // send a standard http response header
              int LED = readString.indexOf("LED=");
             

              if (readString.substring(LED,LED+5) == "LED=T") {
                digitalWrite(LEDpin,HIGH);
                state = "ON";
              }
              else if (readString.substring(LED,LED+5) == "LED=F") {
                digitalWrite(LEDpin,LOW);
                state = "OFF";
              }
             
              if (digitalRead (LEDpin) == HIGH){
                startTime = millis();
              }
             
        if (digitalRead (LEDpin) == LOW){
                stopTime = millis();  
       
        }
            
            
            
            
            
            
            
              client.println("HTTP/1.1 200 OK");
              client.println("Content-Type: text/html");
              client.println("Connection: close");  // the connection will be closed after completion of the response
       client.println("Refresh: 3");  // refresh the page automatically every 3 sec
            
              client.println();

      client.println("<!DOCTYPE HTML>");
              client.println("<html><body bgcolor='Gray'>");
              // Pump Name
              client.println("<center><H1>KO6</H1></center>");
              // output the value of the analog input pin
              for (int analogChannel = 0; analogChannel < 1; analogChannel++) {
                int sensorReading = analogRead(analogChannel);
                sensorReading = map(sensorReading, 0, 1024, 0, 300);
                client.print("<center> Liquid Level ");
                client.print(" is ");
                client.print ("<b><font color='blue'>");
                client.print(sensorReading);
                client.print ("</b></font color>");
                client.println("<br />");
                client.print(" Hours:  ");
               
                client.print(onTime);
                client.println("<br />");     
              }
            
             
              client.print("Pump is ");
              client.print(state);
              client.print("<br><br>");
             
              if (state == "ON") {
                client.println("<a href=\"./?LED=F\">Turn Off<a>");
              }
              else {
                client.println("<a href=\"./?LED=T\">Turn On<a>");
              }
               client.print("</center>");
               client.println("</html>");
              break;
            }
            if (c == '\n') {
              // you're starting a new line
              currentLineIsBlank = true;
            }
            else if (c != '\r') {
              // you've gotten a character on the current line
              currentLineIsBlank = false;
            }
          }
        }
        // give the web browser time to receive the data
        delay(1);
        readString = "";
        // close the connection:
        client.stop();
      }
        }

    [/code]

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I am newbie here but is the problem that you have put this line  " int onTime =+ runTime;" in the declaration section.  It is only ever read once by the program.  Should it not go into the loop()? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I am still a newbie too,

    my theory was to declare "int onTime =+ runTime ;" in the begin so I could use "client.print(onTime);" when I want to out put the run hours on to the webpage.


    I tried " client.print(onTime =+ runTime);" in the loop but I still get a 0 reading .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I am still a newbie too,

    my theory was to declare "int onTime =+ runTime ;" in the begin so I could use "client.print(onTime);" when I want to out put the run hours on to the webpage.


    I tried " client.print(onTime =+ runTime);" in the loop but I still get a 0 reading .