Arduino
  • Products
  • More
Arduino
Arduino Forum is arduino reliable for industrial environment for industrial application?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 52 replies
  • Answers 25 answers
  • Subscribers 423 subscribers
  • Views 10768 views
  • Users 0 members are here
  • dil
Related

is arduino reliable for industrial environment for industrial application?

e14 Contributor
e14 Contributor over 12 years ago

hi all,

i have used arduino uno to make datalogger for industy.i used sd card,rtc,lcd and some basic ic in my circuit.plz do rply.is it reliable to use arduino in industry?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago +6 suggested
    Hello everyone, my name is Daren. I am an Engineer and Arduino software developer. This is the question I started asking when I had clients that needed specialized automation systems for industrial applications…
  • dougw
    dougw over 12 years ago in reply to mcb1 +3 suggested
    I hate to contradict, but can't leave people with an incorrect impression of the ATmega328. This chip does have a watchdog timer and it even has a programming lock for software security. The watchdog can…
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +2 suggested
    Agree with Michael Arduino is an echo system to allow rapid development and education without having to get out the soldering Iron for instance, the boards in general lack the protection circuits often…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    Agree with Michael

     

    Arduino is an echo system to allow rapid development and education without having to get out the soldering Iron for instance, the boards in general lack the protection circuits often required in industrial applications to protect the controller as well as many other potential safety and environmental considerations. I have some experience building systems for the gas industry and in this kind of environment it would not be allowed for instance.

     

    This does not mean that the micro-controller (ATMEGA328 on the UNO) is not suitable for use in industry, you just have to add all the other electronics required to meet the standards. The same goes for TI MCP430 series or other brands. In some areas like Automotive there are very strict requirements which is why you will find a significant percentage of cars use Motorola Micro controllers (Yes they do make them and yes you may never had heard of it). The chips are approved for use in this industry, the approval is expensive but there you go.

     

    As Michael said though, it depends on the specific industry and use and must be evaluated on a case by case basis. If it is a one off then you may simply have to make suitable modifications to the board and container to meet the legislations required for that use. If it is going in a field to measure temp and humidity, there is pretty much not much required except protecting from the elements (Unless the field is in a certain town in England sitting on top of 20M cubic feet of natural gas at 1000PSI  image yes it exists and I put a controller there )

     

    anyway I think you get the idea.

     

    Have fun, be safe

     

    Peter

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mv911
    0 mv911 over 7 years ago in reply to Robert Peter Oakes

    I am working on a project with working of MRF(Magneto Rheological Fluids) & i want to control multiple stepper motors & dc motors, can i use arduino uno  &  if not can you suggest me another device? Thank You, Every help is appreciating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mv911
    0 mv911 over 7 years ago in reply to Robert Peter Oakes

    I am working on a project with working of MRF(Magneto Rheological Fluids) & i want to control multiple stepper motors & dc motors, can i use arduino uno  &  if not can you suggest me another device? Thank You, Every help is appreciating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dougw
    0 dougw over 7 years ago in reply to mv911

    An Uno is fine, although I like the newer, smaller but more powerful MKR series better.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer