Arduino
  • Products
  • More
Arduino
Arduino Forum is arduino reliable for industrial environment for industrial application?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 52 replies
  • Answers 25 answers
  • Subscribers 423 subscribers
  • Views 10780 views
  • Users 0 members are here
  • dil
Related

is arduino reliable for industrial environment for industrial application?

e14 Contributor
e14 Contributor over 12 years ago

hi all,

i have used arduino uno to make datalogger for industy.i used sd card,rtc,lcd and some basic ic in my circuit.plz do rply.is it reliable to use arduino in industry?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago +6 suggested
    Hello everyone, my name is Daren. I am an Engineer and Arduino software developer. This is the question I started asking when I had clients that needed specialized automation systems for industrial applications…
  • dougw
    dougw over 12 years ago in reply to mcb1 +3 suggested
    I hate to contradict, but can't leave people with an incorrect impression of the ATmega328. This chip does have a watchdog timer and it even has a programming lock for software security. The watchdog can…
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +2 suggested
    Agree with Michael Arduino is an echo system to allow rapid development and education without having to get out the soldering Iron for instance, the boards in general lack the protection circuits often…
Parents
  • michaelkellett
    0 michaelkellett over 12 years ago

    It does rather depend on the industry and where you have sourced the parts but I would say that Arduino type parts are not designed for industrial use and are probably not suitable. Electronics for use in induutry will have to satisfy requirements special to the application as well as general requirements such as EMC certification, safetey approvals (if relevant) etc.

     

    On the other hand if your application is a one off piece of test equipment an Arduino based device may be OK.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 12 years ago

    It does rather depend on the industry and where you have sourced the parts but I would say that Arduino type parts are not designed for industrial use and are probably not suitable. Electronics for use in induutry will have to satisfy requirements special to the application as well as general requirements such as EMC certification, safetey approvals (if relevant) etc.

     

    On the other hand if your application is a one off piece of test equipment an Arduino based device may be OK.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to michaelkellett

    Thank you michael.i really need some good place to buy arduino.i have brought it from bang good site.and they cost only 800/arduino.

    is it arduino problem?

    i have used arduino in cable industry in india.in cable industry tempreture is around 40 C

    .is arduino creat problem if earthing not proper?