Arduino
  • Products
  • More
Arduino
Arduino Forum is arduino reliable for industrial environment for industrial application?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 52 replies
  • Answers 25 answers
  • Subscribers 423 subscribers
  • Views 10772 views
  • Users 0 members are here
  • dil
Related

is arduino reliable for industrial environment for industrial application?

e14 Contributor
e14 Contributor over 12 years ago

hi all,

i have used arduino uno to make datalogger for industy.i used sd card,rtc,lcd and some basic ic in my circuit.plz do rply.is it reliable to use arduino in industry?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago +6 suggested
    Hello everyone, my name is Daren. I am an Engineer and Arduino software developer. This is the question I started asking when I had clients that needed specialized automation systems for industrial applications…
  • dougw
    dougw over 12 years ago in reply to mcb1 +3 suggested
    I hate to contradict, but can't leave people with an incorrect impression of the ATmega328. This chip does have a watchdog timer and it even has a programming lock for software security. The watchdog can…
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +2 suggested
    Agree with Michael Arduino is an echo system to allow rapid development and education without having to get out the soldering Iron for instance, the boards in general lack the protection circuits often…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Thank you peter.

    here i put all document which i have regarding my project.i made data logger which store data in sd card this is basic application.

    how whole system work?

    i have used retro reflective sensor to sense the rpm of motor.sensor will give 17v dc when it sense the reflector.after getting this 17v in circuit .i used this 17v and convert it to 5 volt with the help of voltage regulator(7805 and 7812).i used oprocupler ic(MCT 2E) and give 5v to arduino intrupt pin 2.with the help of coding i count the rpm and store it in sd card.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    The only thing I would suggest there is to remove the two regulators your usng to drop the voltage and simply use the  optocoupler

     

    a bit like this

    Fullscreen contentimage_182516.html Download
    <html><head><title>Jive SBS</title></head>
    <body><font face="arial,helvetica,sans-serif">
    <b>Error</b><br><font size="-1">
    An general error occurred while processing your request.
    </font></font></body></html>
    

    just lower the value of the R1 to about 10K should do the trick (It will work with DC too)

     

    you dont need to use the two regulators, just the resistor to limit the current into the opto coupler

     

    I am assuming that the arduino is not powered by this 17V as well

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    The only thing I would suggest there is to remove the two regulators your usng to drop the voltage and simply use the  optocoupler

     

    a bit like this

    Fullscreen contentimage_182516.html Download
    <html><head><title>Jive SBS</title></head>
    <body><font face="arial,helvetica,sans-serif">
    <b>Error</b><br><font size="-1">
    An general error occurred while processing your request.
    </font></font></body></html>
    

    just lower the value of the R1 to about 10K should do the trick (It will work with DC too)

     

    you dont need to use the two regulators, just the resistor to limit the current into the opto coupler

     

    I am assuming that the arduino is not powered by this 17V as well

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 12 years ago in reply to Robert Peter Oakes

    It would be unwise to assume anything.

     

    The ATmega328 in any form has no watchdog timer, hence it can get locked up.

    Any application that requires it working 100% should include a watchdog device to reboot it and warn that it is not running.

     

    You may need to custom design a suitable power supply using switching regulators in order to ensure the 40deg temperatures don't start affecting it.

     

    As Peter and Michael have indicated it depends on the requirements.

    If you're looking for a cheap data logger to provide some information .... then fine.

    If you intend to use this to collect critical data and provide warnings about impending disaster ... then NO.

     

    Mark

     

    Edit

    It seems that there is a WDT and the link shows how you can implement it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to mcb1

    Regarding Watchdog...

     

    Page 1 of the ATMEGA328 user guide http://www.atmel.com/Images/doc8161.pdf

     

    Peripheral Features

    – Two 8-bit Timer/Counters with Separate Prescaler and Compare Mode

    – One 16-bit Timer/Counter with Separate Prescaler, Compare Mode, and Capture Mode

    – Real Time Counter with Separate Oscillator

    – Six PWM Channels

    – 8-channel 10-bit ADC in TQFP and QFN/MLF package

    Temperature Measurement

    – 6-channel 10-bit ADC in PDIP Package

    Temperature Measurement

    – Programmable Serial USART

    – Master/Slave SPI Serial Interface

    – Byte-oriented 2-wire Serial Interface (Philips I2C compatible)

    – Programmable Watchdog Timer with Separate On-chip Oscillator

    – On-chip Analog Comparator

    – Interrupt and Wake-up on Pin Change

    • Special Microcontroller Features

    – Power-on Reset and Programmable Brown-out

     

    10.10.5 Watchdog Timer

    If the Watchdog Timer is not needed in the application, the module should be turned off. If the Watchdog Timer is

    enabled, it will be enabled in all sleep modes and hence always consume power. In the deeper sleep modes, this

    will contribute significantly to the total current consumption. Refer to ”Watchdog Timer” on page 50 for details on

    how to configure the Watchdog Timer

     

    Reset Sources

    The ATmega48A/PA/88A/PA/168A/PA/328/P has four sources of reset:

    • Power-on Reset. The MCU is reset when the supply voltage is below the Power-on Reset threshold (VPOT).

    • External Reset. The MCU is reset when a low level is present on the RESET pin for longer than the minimum

    pulse length.

    • Watchdog System Reset. The MCU is reset when the Watchdog Timer period expires and the Watchdog System

    Reset mode is enabled.

    • Brown-out Reset. The MCU is reset when the supply voltage VCC is below the Brown-out Reset threshold (VBOT)

    and the Brown-out Detector is enabled.

     

    and a howto http://forum.arduino.cc/index.php?topic=128717.0

     

    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 12 years ago in reply to mcb1

    I hate to contradict, but can't leave people with an incorrect impression of the ATmega328. This chip does have a watchdog timer and it even has a programming lock for software security. The watchdog can be accessed in an arduino by including the avr watchdog library. There are many examples on the internet.

    As for using arduinos in industrial applications, it is the same selection process as using any other chip or module - make sure they meet all the required specifications. One weak area to pay particular attention to is the connectors - neither the power connector nor the signal connectors are locking and may not be reliable in a high vibration applications and may have problems with humidity and thermal cycles. This might be improved by using hard-wired solder joints instead of header connectors and you can get arduinos where the cpu is not in a socket but soldered down. Similarly any other weaknesses may be addressed in your system design. For example power supplies are available with any rating you might require and the electronics can be protected from the environment with suitable packaging.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to dougw

    Guys

    Thanks for the update. I stand corrected.

    I always prefer to see a separate chip but I need to do some more digging and thanks for the link.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    no peter arduino is powered by 12v which is driven from 7812ic.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to mcb1

    no i don,t want to collect critical data.i want accuracy around 90%.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    YYou Ned to check the schematics

     

    atmega is either a 5v or a 3.3v device due pending on the model of arduino, in your case it is a 5v device and there is no 7812 on board, maybe a 7805 or a buck regulator for 5v but defiantly not a 12v

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    i have used arduino uno and oprated voltage of arduino is 7-12v.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    you are correct with regard to the voltage applied to the round input power jack but this is not the voltage the actual atmega328 works at (AKA its operating voltage, that is its supply voltage. in the UNO it is a 5V micro-controller device, in other Arduinos it can be 3.3V. If you plug in power via the USB rather than the jack, it is running at a nominal 5V typically, if you supply via the headers it is also 5V or 3V3 depending on the model.

     

    I think I may be miss understanding what your describing, Are you referring to the fact that you have a 12V power supply that is being used to power the Arduino, not the supplies used within the Arduino board itself. In which case, sorry for getting the wroong end of the stick image.

     

    though I would like to point out that using 12V for an extended period of time will cause the on-board regulators to dissipate a lot of heat (More than 50% of the power out of the 12V supply to be precise) as you will be dropping 7V before consuming any of it.

     

    If you can switch out the 12V supply for an economical 5V USB power brick you will be much better off (Assuming this is what your referring to of course)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer