Arduino
  • Products
  • More
Arduino
Arduino Forum Use of Acronyms and Initialisms in discussions
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 21 replies
  • Answers 1 answer
  • Subscribers 422 subscribers
  • Views 3415 views
  • Users 0 members are here
Related

Use of Acronyms and Initialisms in discussions

jw0752
jw0752 over 12 years ago

I am wondering if there is any merit in having a convention for the use of acronyms and initialisms in our discussions? I have been working in electronics for the last 50 plus years but I have not been able to keep up totally with the frontiers or diversity of this science. I have to admit that many times, as I read a description or explanation written by one of the more up-to-date members, I do not understand what they are talking about. The problem is not the ordinary words associated with electronics but rather the PID, TTH, PMBD, ETC. While being able to communicate with such initialisms adds a sense of in-group it is certain to frighten off some of the aspiring beginners as well as the old guys (me). I would propose that when using the Initialism for the first time in a discussion we put it down written out one time first. For example: (We must communicate effectively) WMCE. If "not" WMCE then we are wasting our time. Anyone know if there is a dictionary of electronic initialisms?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 12 years ago +1
    The 722 people who viewed my post have inspired me to take one more step. I have compiled a little over 200 abbreviations, initialisms and acronyms that I will post here. This is just a beginning and I…
  • johnbeetem
    johnbeetem over 12 years ago in reply to e14 Contributor +1
    One of my favorites is PCMCIA: People Cannot Memorize Computer Industry Acronyms
  • mcb1
    mcb1 over 12 years ago in reply to jw0752 +1
    Nice list. When I started at Airways the acronyms were an issue, so I asked if we had a list. 4 A4 pages later was the best they could do, and it wasn't complete. We had a boss once that insisted on using…
Parents
  • shabaz
    0 shabaz over 12 years ago

    Hi John,

     

    Wow, you're dedicated, to have compiled this list : )

     

    It's good that you bring this up.

    I too agree, it's always good practice to see the full expansion at least the first time, and then abbreviations can be acceptable in the rest of the article in question. However, I guess a few are generally accepted, such as V for volt since it is a unit. Hard to know what to do with those.

    There is a school of thought that any two-letter abbreviations are better always expanded throughout the article, rather than only expanding at the first mention of it. So, for example NO and NC should always be expanded to normally open and normally closed, and NO and NC should not appear in an article according to that principle. I don't always follow it 100%, but it's a good guideline and common-sense can be used.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 12 years ago in reply to shabaz

    shabaz wrote:

     

    There is a school of thought that any two-letter abbreviations are better always expanded throughout the article, rather than only expanding at the first mention of it. So, for example NO and NC should always be expanded to normally open and normally closed, and NO and NC should not appear in an article according to that principle. I don't always follow it 100%, but it's a good guideline and common-sense can be used.

    I think the key factors are common sense and know your audience.  If I'm writing about FPGAs in the FPGA group, it's pretty silly and patronizing to expand it as Field-Programmable Gate Array, even the first time.  If it's for a general audience, then I should expand FPGA, though for most people the expanded form doesn't provide that much more information image  (Riiight... what's a gate array?)

     

    As for expanding two-letter initialisms each time: I'm not going to expand IP into Internet Protocol (or Intellectual Property) on each use and I don't think my readers want me to.  The whole point of initialisms is that humans are good at working with symbols and spelling them out unnecessarily gets tiresome IMO.  I love most Dashiell Hammett books, but I find The Glass Key really irritating because the main character is Ned Beaumont and every time DH mentions him it's always "Ned Beaumont".  Never "Ned", never "Beaumont", just Ned Beaumont, Ned Beaumont, Ned Beaumont over and over.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 12 years ago in reply to shabaz

    shabaz wrote:

     

    There is a school of thought that any two-letter abbreviations are better always expanded throughout the article, rather than only expanding at the first mention of it. So, for example NO and NC should always be expanded to normally open and normally closed, and NO and NC should not appear in an article according to that principle. I don't always follow it 100%, but it's a good guideline and common-sense can be used.

    I think the key factors are common sense and know your audience.  If I'm writing about FPGAs in the FPGA group, it's pretty silly and patronizing to expand it as Field-Programmable Gate Array, even the first time.  If it's for a general audience, then I should expand FPGA, though for most people the expanded form doesn't provide that much more information image  (Riiight... what's a gate array?)

     

    As for expanding two-letter initialisms each time: I'm not going to expand IP into Internet Protocol (or Intellectual Property) on each use and I don't think my readers want me to.  The whole point of initialisms is that humans are good at working with symbols and spelling them out unnecessarily gets tiresome IMO.  I love most Dashiell Hammett books, but I find The Glass Key really irritating because the main character is Ned Beaumont and every time DH mentions him it's always "Ned Beaumont".  Never "Ned", never "Beaumont", just Ned Beaumont, Ned Beaumont, Ned Beaumont over and over.