Arduino
  • Products
  • More
Arduino
Arduino Forum Use of Acronyms and Initialisms in discussions
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 21 replies
  • Answers 1 answer
  • Subscribers 422 subscribers
  • Views 3412 views
  • Users 0 members are here
Related

Use of Acronyms and Initialisms in discussions

jw0752
jw0752 over 12 years ago

I am wondering if there is any merit in having a convention for the use of acronyms and initialisms in our discussions? I have been working in electronics for the last 50 plus years but I have not been able to keep up totally with the frontiers or diversity of this science. I have to admit that many times, as I read a description or explanation written by one of the more up-to-date members, I do not understand what they are talking about. The problem is not the ordinary words associated with electronics but rather the PID, TTH, PMBD, ETC. While being able to communicate with such initialisms adds a sense of in-group it is certain to frighten off some of the aspiring beginners as well as the old guys (me). I would propose that when using the Initialism for the first time in a discussion we put it down written out one time first. For example: (We must communicate effectively) WMCE. If "not" WMCE then we are wasting our time. Anyone know if there is a dictionary of electronic initialisms?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 12 years ago +1
    The 722 people who viewed my post have inspired me to take one more step. I have compiled a little over 200 abbreviations, initialisms and acronyms that I will post here. This is just a beginning and I…
  • johnbeetem
    johnbeetem over 12 years ago in reply to e14 Contributor +1
    One of my favorites is PCMCIA: People Cannot Memorize Computer Industry Acronyms
  • mcb1
    mcb1 over 12 years ago in reply to jw0752 +1
    Nice list. When I started at Airways the acronyms were an issue, so I asked if we had a list. 4 A4 pages later was the best they could do, and it wasn't complete. We had a boss once that insisted on using…
Parents
  • shabaz
    0 shabaz over 12 years ago

    Hi John,

     

    Wow, you're dedicated, to have compiled this list : )

     

    It's good that you bring this up.

    I too agree, it's always good practice to see the full expansion at least the first time, and then abbreviations can be acceptable in the rest of the article in question. However, I guess a few are generally accepted, such as V for volt since it is a unit. Hard to know what to do with those.

    There is a school of thought that any two-letter abbreviations are better always expanded throughout the article, rather than only expanding at the first mention of it. So, for example NO and NC should always be expanded to normally open and normally closed, and NO and NC should not appear in an article according to that principle. I don't always follow it 100%, but it's a good guideline and common-sense can be used.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to shabaz

    JAFMA image

     

    The interesting part with acronyms is that you'll often find that two people with a differing history of companies they've worked for will have wildly different interpretations for the same TLA, or equally two totally different ones for the same thing. For example, two places I worked for used CND and NFF for essentially the same thing. I try to avoid using TLAs for reasons like this, I'm probably not totally successful though image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 12 years ago in reply to e14 Contributor

    One of my favorites is PCMCIA: People Cannot Memorize Computer Industry Acronyms image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 12 years ago in reply to e14 Contributor

    I was trying to guess CND/NFF and all I could think of was Campaign for Nuclear Disarmament, and then Nuclear Failure something as a guess : ) I needed to type it into google to find out what it really meant. The places I've worked, it would be a single-letter abbreviation, "U" (Unreproducible) if I've interpreted it correctly.

     

    I can see the point that sometimes it's not desirable to expand, e.g. FPGA in an FPGA group, and guidelines are made to be sometimes broken. Sometimes I've found an audience is really not aware of certain abbreviations or even buzzwords, although I thought they should have been aware (i.e. my bad judgement - and it gets harder with technology that is just a year or two old, it might not have permeated as quickly as I had thought). It's a hard balance. Others I've forgotten (like TRIAC - I know what it is, but not what the abbreviation is any longer) due to passage of time. But then, possibly people don't need to know what TRIAC stands for, since it has almost become a word (much like RADAR). I just checked what TRIAC stands for, and it could be an anachronism to today try to understand the expansion.

    So there are loads of subtleties to be factored in and always exceptions to guidelines.

     

    I also see extremely long abbreviations like EoMPLSoGRE and they are generally expanded the first time, although it may be done in sections (i.e. EoMPLS is expanded and discussed, and then the oGRE bit is expanded.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to shabaz

    shabaz wrote:

     

    I was trying to guess CND/NFF and all I could think of was Campaign for Nuclear Disarmament, and then Nuclear Failure something as a guess : ) I needed to type it into google to find out what it really meant. The places I've worked, it would be a single-letter abbreviation, "U" (Unreproducible) if I've interpreted it correctly.

    Sounds like you've got it right, but perfect example is that you have yet another way to denote the same thing.

     

    When I used to work for a subcontract board manufacturer we used CND and could never work out why one of our customers sent some percentage of failed boards back to us labeled NFF. Later I changed job and started working for that same customer and discovered what NFF meant to them, and therefore also that whoever they had sorting out the returns didn't understand the acronym either!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to e14 Contributor

    I think the couple from "Blue Thunder" are also interesting.

    SNAFU  Situation Normal All F ... Up.

    JAFO Just Another F... Observer.

     

     

    We have a couple that catch our newbies out.

    RNO Return to Normal Operation.

    U/S  unserviceable

    DG Diesel Generator

    LVO Low Visibility Operations

    UPS Uninterrupted Power Supply, however it got confusing when the manufacturer also used the same but meant Universal Power Supply

     

     

    mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to mcb1

    mcb1 wrote:

    I think the couple from "Blue Thunder" are also interesting.

    JAFO Just Another F... Observer.

     

    Yay, someone got the JAFMA reference image   Damn, now I'm feeling old image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to mcb1

    mcb1 wrote:

    I think the couple from "Blue Thunder" are also interesting.

    JAFO Just Another F... Observer.

     

    Yay, someone got the JAFMA reference image   Damn, now I'm feeling old image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • neilk
    0 neilk over 12 years ago in reply to e14 Contributor

    My own favourite, when having failed to get a piece of equipment or software to work, is RTFM