Arduino
  • Products
  • More
Arduino
Arduino Forum Sine PWM generation using Arduino UNO
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 419 subscribers
  • Views 2414 views
  • Users 0 members are here
  • spwm
Related

Sine PWM generation using Arduino UNO

e14 Contributor
e14 Contributor over 12 years ago

Dear all

 

I am a University student and I have been assigned with a project of developing an Inverter circuit. Therefore, I need to generate a SPWM control signal for my switches.

In the past years I was involved with Arduino programming but never got into interrupts and timers. So I reached a dead end since I have no idea of how to program the Arduino to generate a sine PWM signal. I have been through several codes found on the internet and they worked perfectly. Thing is that I need to understand them cause I need to make some changes.

I would really appreciate your help.

 

Kind Regards

D.M.

 

P.S. I am attaching the code found on-line

Attachments:
spwm.ino.zip
  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 12 years ago

    The code you posted just uses a look up table to make sines from phase angles and a DDS (google it) to make the phase angles. If you want to run your inverter at  a constant frequency you don't need to bother with the DDS, just make a table of pulse widths and step though it at  a constant rate. You should synchronize the PW changes with the PWM frequency  - it might be worth interpolating between sine values from a table to avoid steps in the PWM settings.  I don't use Arduinos so I'm not sure if you have the level of control you would get in C or Assembler.

    Is your project more concerned with hardware or software ?

    What hardware are you using for the inverter itself.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to michaelkellett

    Thank you for your quick response. I am doing both hardware and software, and now i am at a stage where i have developed my hardware part and i am experimenting with the software. i am using MOSFET switches along with opto-couplers and drivers.

    i would like to thank you again for your advice but I am looking for an explanatory guidance through the program itself, so i can find what is responsible for the output frequency, how I can invert the signal (without the use of logic gates) and guide it through a different output and how can i integrate a pwm algorithm independent from the control signal in order to control a couple of other switches! I know it may sound confusing but the general idea is to generate a SPWM signal for the H-bridge circuit, separate the positive from the negative half cycle. Along with that, I need another square pulse for additional purposes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to e14 Contributor

    You're going to have to unpick the programme yourself to really understand it. Have you looked up DDS synthesiser yet (there's a lot on the web some of the stuff on Analog Devices' website is helpful).

    I doubt very much that the Arduino can generate complementary PWM outputs - you would need a much more modern micro with better timers - are you stuck with the Arduino  or could you use an ARM Cortex (the ST parts (and others)) have much more sophisticated timers with complementary outputs, dead time control, emergency stop etc.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to e14 Contributor

    You're going to have to unpick the programme yourself to really understand it. Have you looked up DDS synthesiser yet (there's a lot on the web some of the stuff on Analog Devices' website is helpful).

    I doubt very much that the Arduino can generate complementary PWM outputs - you would need a much more modern micro with better timers - are you stuck with the Arduino  or could you use an ARM Cortex (the ST parts (and others)) have much more sophisticated timers with complementary outputs, dead time control, emergency stop etc.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to michaelkellett

    I was just reading about this capability with the TivaC Connected Launch pad last night, it has very sophisticated timers and has all the above features and quadrature Encoder input for speed and direction sensing as well. A very powerful chip and quite an extensive support library