Arduino
  • Products
  • More
Arduino
Arduino Forum Security camera for cars
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 416 subscribers
  • Views 293 views
  • Users 0 members are here
  • bluetooth
  • camera
  • arduino
Related

Security camera for cars

e14 Contributor
e14 Contributor over 12 years ago

Hi all,

We are building this project that is a security camera for cars. y-bus.com/camera

It takes pictures everytime the car breaks and sends it to the internet! It is a great solution for dangerous Latin American cities like Rio de Janeiro.

 

We are using a Arduino Yun to connect to the mobile phone hotspot (wifi) and it is kind of hard and the Yun keeps loosing connection.

 

I would like to make it easier for the user to connect. I was thinking using bluetooth or attaching a camera into the mobile phone.

 

Can anyone help me?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I like your idea, but there are some things you should put in mind. It would be better if you could have the an integrated mobile network connection ( you don't want your consumer to have to connect his or her phone or probably loose battery fast. ), and also you may want to make a local storage and probably send the image by increments due to mobile network signals to be bad at some points, probably make it send when you have a good solid connection. P.S. For cars its called brakes, not breaks. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I was able to create a prototype with local storage using the wifi hotspot.

    But I thinking to use a bluetooth connection just like a phone connect to the speakers of the car.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I was able to create a prototype with local storage using the wifi hotspot.

    But I thinking to use a bluetooth connection just like a phone connect to the speakers of the car.