Arduino
  • Products
  • More
Arduino
Arduino Forum I need help with switching signals
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 418 subscribers
  • Views 1320 views
  • Users 0 members are here
  • pins
  • signals
  • switch
Related

I need help with switching signals

e14 Contributor
e14 Contributor over 12 years ago

Hi there

Although I know a thing or two (ok, maybe 1.5 things) about soldering, I am fairly new to this electronics thing. I've been thinking about starting a secret project that I will only share once I finish. I had trouble finding the materials I need such as the battery, the charging mechanism, ...etc. That is not important right now. As I was listing down the things I wanted it to do, I encountered something I don't know how to solve, thus I need your guys' help

Say I'm connecting two points together (let's call them A and B). Now, I need to switch the output from B to another point called D that gets it's signal from point C by pressing a button. Basically I want to flip the signals (you can think of it as cross multiply in math terms) Now you could say "just use a slide switch, you dummy" but the problem is I have 60 inputs and outputs. do you think you can help me with this?

I thought of using an EEPROM because they have a lot of pins so that I would only need to use 2 of them, but I know nothing on how to program them. I would assume a micro controller would be better but I don't know how to program it either, and I assume it's not as cheap as an EEPROM. I also have no experience in using an arduino. I do, however, know the basics of java, so if that helps please tell me

I really wanna do this. I've been thinking about it for quite a while. Please help.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    What you need is a switch or a multiplexer, providing your signals are logic levels, this should work look at something like this : for digital signals use a 74157 (No uProc needed) http://mazharlaliwala…
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    What you need is a switch or a multiplexer, providing your signals are logic levels, this should work

     

    look at something like this : for digital signals use a 74157 (No uProc needed)  http://mazharlaliwala.wordpress.com/2011/07/13/nibble-multiplexer/

     

    there are many variety's so just Google away for alternatives

     

    Hope this hep

     

    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 12 years ago

    Hi Ehab, I have a few questions. Are the 60 switches all controlled separately by push buttons? Will you be switching more than one at once? When you say that you are switching signals are they digital or analog? Do the switches have to be bidirectional? B to D only , D to B only or both ways? When you say that you are connecting point B to D does this mean that you are disconnecting it from A at the same time? Does this mean that the signal from C is also switched to A? When you ask a very general question like this you can only receive a more general answer. I know you want to protect your idea but in order for anyone to give you a more exact answer you will have to be more specific in your questions and also provide enough collateral detail so good advice can be returned to you. Adding a diagram often helps to clarify a question.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago
    What you need is a switch or a multiplexer, providing your signals are logic levels, this should work

    I did think about that option during a break between my classes. The problem is that I will need a lot of them to switch all 60 signals at the same time, and I need it to be as small as possible

     

    Are the 60 switches all controlled separately by push buttons? Will you be switching more than one at once? When you say that you are switching signals are they digital or analog? Do the switches have to be bidirectional? B to D only , D to B only or both ways? When you say that you are connecting point B to D does this mean that you are disconnecting it from A at the same time? Does this mean that the signal from C is also switched to A?

    I made a little animation to help describe what I'm trying to achieve (hope it helps!)

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    Note: I left two pins on both controllers disconnected as I think they will be connected to the switch. Meaning that each controller will have 32 pins. Do they make controllers with that many pins?

     

    EDIT: I forgot to mention that the signals are digital

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 12 years ago

    Hi Ehab,  The diagram was excellent and should get us some help from one of the more experienced guys on the forum. Each element of your switch looks like a cross wired DPDT switch. The only chip I am aware of that has this type of switch is an AD7512 (I've worked with this one) and it only has one DPDT so you would need 30 of them. The AD7512 is a bidirectional analog switch. It has about 75 ohms of internal resistance and can switch about 20 mA. Hopefully there is a chip with internal design to do this specifically on a larger scale. Your clarification should help to get a better answer than I can give you.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to jw0752

    Since the signals are digital it can be done easily with an FPGA.

     

    You will need one with at least 128 useable IO pins, 120 for the switch IO and some for control.

    (Or possibly 2 because then they might be in more manageable packages.)

     

    Can you explain a bit more about what this is for because it may be that there is a much simpler solution if we understood a bit more.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    like I said in my latest post, the signals are digital. At least I think so.
    the 60 pins actually come from a console. an NES to be exact. I believe the reason why I want to do this is self explanatory for those who know a little about the console

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to e14 Contributor

    I just noticed that they were digital and was editing my reply when you answered.

     

    What sort of signals are they - voltage levels, speed etc. An I know a fair bit about electronics but nothing at all about 'consoles' or even what an 'NES' is - so you need to explain.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to michaelkellett

    honestly, I don't know. As I explained, I am not that good with electronics. I figured that all signals would all be the same since they're (according to my understanding) just a series of binary numbers. I can provide you with the names of the pins, if that helps

     

    Basically, what happens with a cartridge based console, is the console powers up the cartridge with (in the case of the Nintendo Entertainment System aka NES) 5V, and then the cartridge sends signals from two EEPROMs on it to the console.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to e14 Contributor

    You still haven't explained what you want to do !

     

    If it's 5V logic (and it could be because the NES is such old technology) then you can forget about FPGA's because they won't work with 5V.

     

    Are you trying to select between two different cartridges -  if so it may well not be necessary to switch all the signals but just make sure that only one cartridge is enabled at a time.

     

    If you can explain what you are trying to make or do it may be possible to help.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    alright, I'll tell you
    The japanese version of the NES has different sized cartridges (that include the number of pins). The pins are also placed differently. What I want to do is to be able to push a button to change/switch the bridges between the cartridge and the console. Which is why the arrows cross in the given video.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>