Arduino
  • Products
  • More
Arduino
Arduino Forum having trouble with ieeflip vfd and ieeflipnofrills
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 417 subscribers
  • Views 955 views
  • Users 0 members are here
  • displays
  • iee
  • help
  • library
  • ieeflip
  • ieeflipnofrills
  • vfd
  • arduino
Related

having trouble with ieeflip vfd and ieeflipnofrills

e14 Contributor
e14 Contributor over 12 years ago

First off, i am new to the arduino world of open source tech. I really like MAKE magizine and it as well as a co worker of mine has gave me the push i needed to get into open souce hardware and codeing.  i have been playing with the arduino now for about 2 or 3 months now and have got to the point where i want to learn displays.

 

second, i have a ieeflip vfd 03601-02-040, that was source from some old parts laying around. i wanted to make it display the time and date and day of the week.

 

third,  i have a rtc and a arduino uno. i chopped the example code that came with the rtc library down to what i needed to do and it works pretty good. so it came time for me to wire up the vfd and import the vfd libraries. so i downloaded the IeeFlipNoFrills library from arduino.cc i wired up the display in accordance to what the hello world example said and im getting a few errors maybe you guys could help me out with.


please keep in mind that in new to this. lol thanks

 

 

this is the code:

 

/*

  IeeFlipNoFrills Library - Hello World

 

Demonstrates the use an IEE Flip "No Frills" VFD. Tested

with model 03601-95A-40 2x20 alphanumeric display.

 

This sketch prints "Hello World!" to the VFD

and shows the number of seconds since the sketch

started.

 

  The circuit:

 

* Display pins 1 (BUSY) connected to Arduino pin 2

* Display pins 2 (WRITE STROBE) connected to Arduino pin 3

* Display pins 3-10 (D7-D0) connected to Arduino pins 4-11

* Display pin 11 (+5V @ 370mA) connected to +5V

* Display pin 12 (GND) connected to GND

* Display pins 13 & 14 unconnected

 

Created Mar 6, 2011.

Ported to IeeFlipNoFrills on April 10, 2011.

 

This example code is in the public domain.

 

http://arduino.cc/playground/Main/IeeFlipNoFrills

*/

 

// Include the library code.

#include <IeeFlipNoFrills.h>

 

// Initialize the library with the numbers of the interface pins

IeeFlipNoFrills vfd(2, 3, /* control pins */

                    11, 10, 9, 8, 7, 6, 5, 4 /* data pins */);

           

void setup() {

  // Start the library/displaying to the vfd

  vfd.begin(20, 2);

  // Print a message to the VFD.

  vfd.print("hello, world!");

}

 

void loop() {

 

  // Set the cursor to the first column (0) of the second row (1).

  vfd.setCursor(0, 1);

  // Print the number of seconds since reset.

  vfd.print(millis()/1000);

}

 

 

and this is the error message:

 

 

In file included from HelloWorld.pde:29:

/home/chris/sketchbook/libraries/IeeFlipNoFrills/IeeFlipNoFrills.h:16:22: error: WProgram.h: No such file or directory

In file included from HelloWorld.pde:29:

/home/chris/sketchbook/libraries/IeeFlipNoFrills/IeeFlipNoFrills.h:83: error: conflicting return type specified for ‘virtual void IeeFlipNoFrills::write(uint8_t)’

/home/chris/Desktop/arduino-1.0.5/hardware/arduino/cores/arduino/Print.h:48: error:   overriding ‘virtual size_t Print::write(uint8_t)’

  • Sign in to reply
  • Cancel

Top Replies

  • kidiccurus
    kidiccurus over 12 years ago +1
    Check you have the library installed properly using the example sketch. If it doesn't work, delete and reinstall your library.
  • kidiccurus
    0 kidiccurus over 12 years ago

    Check you have the library installed properly using the example sketch. If it doesn't work, delete and reinstall your library.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to kidiccurus

    ive done that a couple times. i read that i might try installing a older version like arduino 0023 and load the library in that install and go from there, i tried that and it gave me a java error upon compiling. i am currently running linux ubuntu and doing things with linux is a little new to me but its all pretty straight forward like mac and microsoft. look like i may need to get out the old vista laptop and give her a go.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    the sketch posted is the example sketch fyi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 12 years ago in reply to e14 Contributor

    Something being compatiblewith vista?? Odd concept. Try checking your circuit, it may be your wiring or display at fault and if that does not work try to find a new libary, or even write your own. Unfortunately, getting libraries to work is really hard, as I found out when trying to interface with an n64 controller. In the end I gave up and used an nes controller instead.