Arduino Forum having trouble with ieeflip vfd and ieeflipnofrills
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
  • State Not Answered
  • Replies 4 replies
  • Subscribers 402 subscribers
  • Views 796 views
  • Users 0 members are here
  • displays
  • iee
  • help
  • library
  • ieeflip
  • ieeflipnofrills
  • vfd
  • arduino
Related

having trouble with ieeflip vfd and ieeflipnofrills

Former Member
Former Member over 11 years ago

First off, i am new to the arduino world of open source tech. I really like MAKE magizine and it as well as a co worker of mine has gave me the push i needed to get into open souce hardware and codeing.  i have been playing with the arduino now for about 2 or 3 months now and have got to the point where i want to learn displays.

 

second, i have a ieeflip vfd 03601-02-040, that was source from some old parts laying around. i wanted to make it display the time and date and day of the week.

 

third,  i have a rtc and a arduino uno. i chopped the example code that came with the rtc library down to what i needed to do and it works pretty good. so it came time for me to wire up the vfd and import the vfd libraries. so i downloaded the IeeFlipNoFrills library from arduino.cc i wired up the display in accordance to what the hello world example said and im getting a few errors maybe you guys could help me out with.


please keep in mind that in new to this. lol thanks

 

 

this is the code:

 

/*

  IeeFlipNoFrills Library - Hello World

 

Demonstrates the use an IEE Flip "No Frills" VFD. Tested

with model 03601-95A-40 2x20 alphanumeric display.

 

This sketch prints "Hello World!" to the VFD

and shows the number of seconds since the sketch

started.

 

  The circuit:

 

* Display pins 1 (BUSY) connected to Arduino pin 2

* Display pins 2 (WRITE STROBE) connected to Arduino pin 3

* Display pins 3-10 (D7-D0) connected to Arduino pins 4-11

* Display pin 11 (+5V @ 370mA) connected to +5V

* Display pin 12 (GND) connected to GND

* Display pins 13 & 14 unconnected

 

Created Mar 6, 2011.

Ported to IeeFlipNoFrills on April 10, 2011.

 

This example code is in the public domain.

 

http://arduino.cc/playground/Main/IeeFlipNoFrills

*/

 

// Include the library code.

#include <IeeFlipNoFrills.h>

 

// Initialize the library with the numbers of the interface pins

IeeFlipNoFrills vfd(2, 3, /* control pins */

                    11, 10, 9, 8, 7, 6, 5, 4 /* data pins */);

           

void setup() {

  // Start the library/displaying to the vfd

  vfd.begin(20, 2);

  // Print a message to the VFD.

  vfd.print("hello, world!");

}

 

void loop() {

 

  // Set the cursor to the first column (0) of the second row (1).

  vfd.setCursor(0, 1);

  // Print the number of seconds since reset.

  vfd.print(millis()/1000);

}

 

 

and this is the error message:

 

 

In file included from HelloWorld.pde:29:

/home/chris/sketchbook/libraries/IeeFlipNoFrills/IeeFlipNoFrills.h:16:22: error: WProgram.h: No such file or directory

In file included from HelloWorld.pde:29:

/home/chris/sketchbook/libraries/IeeFlipNoFrills/IeeFlipNoFrills.h:83: error: conflicting return type specified for ‘virtual void IeeFlipNoFrills::write(uint8_t)’

/home/chris/Desktop/arduino-1.0.5/hardware/arduino/cores/arduino/Print.h:48: error:   overriding ‘virtual size_t Print::write(uint8_t)’

  • Sign in to reply
  • Cancel

Top Replies

  • kidiccurus
    kidiccurus over 11 years ago +1
    Check you have the library installed properly using the example sketch. If it doesn't work, delete and reinstall your library.
Parents
  • kidiccurus
    0 kidiccurus over 11 years ago

    Check you have the library installed properly using the example sketch. If it doesn't work, delete and reinstall your library.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to kidiccurus

    ive done that a couple times. i read that i might try installing a older version like arduino 0023 and load the library in that install and go from there, i tried that and it gave me a java error upon compiling. i am currently running linux ubuntu and doing things with linux is a little new to me but its all pretty straight forward like mac and microsoft. look like i may need to get out the old vista laptop and give her a go.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    the sketch posted is the example sketch fyi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    the sketch posted is the example sketch fyi