Arduino
  • Products
  • More
Arduino
Arduino Forum How to wire a transistor?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Answers 2 answers
  • Subscribers 418 subscribers
  • Views 2178 views
  • Users 0 members are here
  • transistor
  • circuit
  • wiring
  • wire
  • Design
  • arduino
  • circuitry
Related

How to wire a transistor?

nschreiber0813
nschreiber0813 over 12 years ago

Dear: Element 14

Hello it is me Noah again as you may remember me from my last post I am trying to build an arduino rocket controller and I am at prototyping stage. First of all you should know that I am using transistors BD712 which a pnp transistor that I need to amplify a current. The reason I need it to amplify a current is because I need it to increase 5V to 7.5V and to then send the current to my fixed barrier terminal blocks where it will then detonate the rocket motors. You see first of all in order you need a base resistor that connects to ground. The reason you need that is to prevent the board from short circuiting. I have placed several base resistors at several points and according to wikipedia I think I am doing this right. It says on wikipedia that I should do this.

NPN_common_emitter.svg

And this is what I did.

image

Please can you help me because I am not even sure what a transistor is?

  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 12 years ago +1
    It would be useful to know how much current you would need to actuate an ignitior, and if they melt open when actuated. If this is the case, you could use a thrystor. In the more general case of having…
  • D_Hersey
    D_Hersey over 12 years ago +1
    Sure, thank you kindly for asking. I used to play with rockets when I was a kid, but feel free to enlighten me on the topic. A thrystor is a device such as a SCR or TRIAC. These devices turn on well, but…
  • D_Hersey
    D_Hersey over 12 years ago +1
    Model rocket igniters are made with wires made from nichrome, or were when I was a kid. The electric burner on a stove is made out of the stuff AFIK. It is 50/50 nickel and chrome. Hard, low corrosive…
Parents
  • D_Hersey
    0 D_Hersey over 12 years ago

    Model rocket igniters are made with wires made from nichrome, or were when I was a kid.  The electric burner on a stove is made out of the stuff AFIK.  It is 50/50 nickel and chrome.  Hard, low corrosive and high bulk resistivity for a metal.  So it is used in heating elements.  When drawn into wire it has a rather definite ohms/foot.  Back in the old days it was also used to make model locos smoke by heating up some stuff.

     

    SCRs and TRIACs are devices that can be turned on (sorta) like a transistor but cannot be turned off by their control terminals.  You could google them.

     

    The ADJ terminal is like a signal input.  The OUTPUT terminal will source (or sink, depending) current in an attempt to keep it 1.2V above ground.  So, for example, if we jumped ADJ to GND, the pass Q would turn all of the way on.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 12 years ago

    Model rocket igniters are made with wires made from nichrome, or were when I was a kid.  The electric burner on a stove is made out of the stuff AFIK.  It is 50/50 nickel and chrome.  Hard, low corrosive and high bulk resistivity for a metal.  So it is used in heating elements.  When drawn into wire it has a rather definite ohms/foot.  Back in the old days it was also used to make model locos smoke by heating up some stuff.

     

    SCRs and TRIACs are devices that can be turned on (sorta) like a transistor but cannot be turned off by their control terminals.  You could google them.

     

    The ADJ terminal is like a signal input.  The OUTPUT terminal will source (or sink, depending) current in an attempt to keep it 1.2V above ground.  So, for example, if we jumped ADJ to GND, the pass Q would turn all of the way on.