Arduino
  • Products
  • More
Arduino
Arduino Forum How to connect a cellular antenna?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 419 subscribers
  • Views 1486 views
  • Users 0 members are here
  • rover_5
  • bluetooth
  • connector
  • gps
  • cellular_antenna
  • wireless
  • arduino
Related

How to connect a cellular antenna?

nschreiber0813
nschreiber0813 over 12 years ago

Dear: Element 14

First of all you should know that I am currently working on my Rover 5 chassis. I would like my rover 5 chassis to have a GPS so it doesn't get lost and for it to also have a Bluetooth module so I can control it remotely and autonomously. But in order to do that I need an antenna. See the antennas on both modules aren't powerful enough to send a signal back and to receive it. That is why I am using part cel-0075 which you can find here. Good luck I could use all the help I can get.

From: Noahimage

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +1 suggested
    Noah, I don't think this is going to work the way you expect. As I understand your question, you want to control your rover via bluetooth (which operates at 2.4 GHz) via a cellular antenna, which operates…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to nschreiber0813 +1
    Noah, You'll need a pigtail to connect the antenna to the board. Something like this: http://www.amazon.com/TP-LINK-TL-ANT24PT-RP-SMA-Pigtail-Cable/dp/B003U6825G/ref=sr_1_5?ie=UTF8&qid=1407111497&sr=8…
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    Noah What controller are you planning to use on this project, You should know that a lot of the Arduino's will not be able to talk to a USB Bluetooth dongle (adapter) like the one you linked in, you will…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Noah,


    I don't think this is going to work the way you expect.  As I understand your question, you want to control your rover via bluetooth (which operates at 2.4 GHz) via a cellular antenna, which operates at 900 MHz?  You'll need either a bluetooth antenna (standard 2.4 GHz wifi antenna should suffice) to connect to your bluetooth module, or you'll need a cellular module to hook the cel-0075 up to, such as http://www.amazon.com/dp/B00A8DDYB6/ref=wl_it_dp_o_pC_nS_ttl?_encoding=UTF8&colid=2B8RER3KNREL5&coliid=IA0DRG4ESCEJL

     

    There may be ways to connect that antenna to the bluetooth module, but given the antenna is "tuned" for a different frequency, it likely won't help much.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Noah,


    I don't think this is going to work the way you expect.  As I understand your question, you want to control your rover via bluetooth (which operates at 2.4 GHz) via a cellular antenna, which operates at 900 MHz?  You'll need either a bluetooth antenna (standard 2.4 GHz wifi antenna should suffice) to connect to your bluetooth module, or you'll need a cellular module to hook the cel-0075 up to, such as http://www.amazon.com/dp/B00A8DDYB6/ref=wl_it_dp_o_pC_nS_ttl?_encoding=UTF8&colid=2B8RER3KNREL5&coliid=IA0DRG4ESCEJL

     

    There may be ways to connect that antenna to the bluetooth module, but given the antenna is "tuned" for a different frequency, it likely won't help much.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • nschreiber0813
    0 nschreiber0813 over 12 years ago in reply to e14 Contributor

    Dear: John

    Thank you for your last post. That was especially helpful because I didn't know I was using the wrong antenna. I am sorry but I have to ask you can you point out any brands that don't come with a board because I am making a custom PCB from scratch as you should know. Good Luck!!!image

    From: Noah

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nschreiber0813
    0 nschreiber0813 over 12 years ago in reply to e14 Contributor

    Never-mind sorry to make you look but I found an antenna right here but I still need some questions to be answered.image