Arduino
  • Products
  • More
Arduino
Arduino Forum How to connect a cellular antenna?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 419 subscribers
  • Views 1486 views
  • Users 0 members are here
  • rover_5
  • bluetooth
  • connector
  • gps
  • cellular_antenna
  • wireless
  • arduino
Related

How to connect a cellular antenna?

nschreiber0813
nschreiber0813 over 12 years ago

Dear: Element 14

First of all you should know that I am currently working on my Rover 5 chassis. I would like my rover 5 chassis to have a GPS so it doesn't get lost and for it to also have a Bluetooth module so I can control it remotely and autonomously. But in order to do that I need an antenna. See the antennas on both modules aren't powerful enough to send a signal back and to receive it. That is why I am using part cel-0075 which you can find here. Good luck I could use all the help I can get.

From: Noahimage

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +1 suggested
    Noah, I don't think this is going to work the way you expect. As I understand your question, you want to control your rover via bluetooth (which operates at 2.4 GHz) via a cellular antenna, which operates…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to nschreiber0813 +1
    Noah, You'll need a pigtail to connect the antenna to the board. Something like this: http://www.amazon.com/TP-LINK-TL-ANT24PT-RP-SMA-Pigtail-Cable/dp/B003U6825G/ref=sr_1_5?ie=UTF8&qid=1407111497&sr=8…
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    Noah What controller are you planning to use on this project, You should know that a lot of the Arduino's will not be able to talk to a USB Bluetooth dongle (adapter) like the one you linked in, you will…
Parents
  • nschreiber0813
    0 nschreiber0813 over 12 years ago

    Dear: Element 14

    You should know I found this cellular antenna off the internet. What connector will fit it I am not getting that. What does "Changing Gender" mean I am not getting that either.

    From: Noahimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to nschreiber0813

    Noah,

     

    You'll need a pigtail to connect the antenna to the board.  Something like this:  http://www.amazon.com/TP-LINK-TL-ANT24PT-RP-SMA-Pigtail-Cable/dp/B003U6825G/ref=sr_1_5?ie=UTF8&qid=1407111497&sr=8-5&keywords=pigtail

     

    The large end will connect to the antenna, and the small end will connect to the external antenna connection on the module you're using the antenna with.  Since you mentioned the CSR 4.0 (which has this chipset:  http://www.csr.com/products/54/csr8000-platform ), I don't know if you'll be able to connect the pigtail directly, you may have to solder it in (Sorry, unable to help there).

     

    Edit - as for "changing gender", the connectors will either be male or female, and if you run into a situation where you need to connect two similar connectors, you'll need a "gender change" adapter so you can connect them together.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to nschreiber0813

    Noah,

     

    You'll need a pigtail to connect the antenna to the board.  Something like this:  http://www.amazon.com/TP-LINK-TL-ANT24PT-RP-SMA-Pigtail-Cable/dp/B003U6825G/ref=sr_1_5?ie=UTF8&qid=1407111497&sr=8-5&keywords=pigtail

     

    The large end will connect to the antenna, and the small end will connect to the external antenna connection on the module you're using the antenna with.  Since you mentioned the CSR 4.0 (which has this chipset:  http://www.csr.com/products/54/csr8000-platform ), I don't know if you'll be able to connect the pigtail directly, you may have to solder it in (Sorry, unable to help there).

     

    Edit - as for "changing gender", the connectors will either be male or female, and if you run into a situation where you need to connect two similar connectors, you'll need a "gender change" adapter so you can connect them together.