Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino boot loader question
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 417 subscribers
  • Views 320 views
  • Users 0 members are here
Related

Arduino boot loader question

e14 Contributor
e14 Contributor over 12 years ago

I purchased some atmel 328 chips with the boot loader programed in them.

 

I replaced the chip in my uno with one of these chips. It doesn't work. Whats going on?

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    I suspect it may not have a boot loader in it

     

    Do you have an ISP programmer (Connects to the six pin header on the arduino), if so then you can simply add you own bootloader

     

    If your VERY new to hardware, make sure the chip is plugged in the right way , if it was the wrong way, you may have damaged it but you could also be lucky

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to Robert Peter Oakes

    You also need to clarify which bootloader it has loaded.

    There are two versions and some of the asian sourced UNO's use an USB to serial chip rather than the Atmega 8U or 16U chip.

     

    In theory the Duemilanove programs slower so should work, but I haven't tried it.

     

    some info here.

    Arduino - ArduinoBoardUno

    Arduino - ArduinoBoardDuemilanove

     

    Can you post the link to where you obtained these chips, and possibly the error message you get.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 12 years ago in reply to Robert Peter Oakes

    You also need to clarify which bootloader it has loaded.

    There are two versions and some of the asian sourced UNO's use an USB to serial chip rather than the Atmega 8U or 16U chip.

     

    In theory the Duemilanove programs slower so should work, but I haven't tried it.

     

    some info here.

    Arduino - ArduinoBoardUno

    Arduino - ArduinoBoardDuemilanove

     

    Can you post the link to where you obtained these chips, and possibly the error message you get.

     

    Mark