Arduino
  • Products
  • More
Arduino
Arduino Forum Help with motor driver module
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 418 subscribers
  • Views 1560 views
  • Users 0 members are here
Related

Help with motor driver module

jehielmartinez
jehielmartinez over 12 years ago

I make an Arduino standalone to drive a simple bluetooth RC Car from my Android phone. Using a

ZITRADES L9110S DC/Stepper Motor Driver Module, a Tamiya double motor gearbox and a HC-06 Bluetooth module.


When I run my code on the Microcontroller eveything works fine, then I plug the Motor Driver  and everything fails.

I need help with this issue? I dont know what's the problem.

I plug just one motor and works, but it doesnt works with the two motors plugged on the Driver Module.

T


  • Sign in to reply
  • Cancel
Parents
  • jehielmartinez
    0 jehielmartinez over 12 years ago

    Thank you for your reply.

    Here's the problem more detalied. Sorry for the crappy solder job. I was soldering and desoldering things trying to fix it

    image

    image

    WHEN I CONNECT  THE MOTOR DRIVER VCC TO THE POSITIVE JOINT ON THE BATTERY PACK WITH A ALLIGATOR CLIP. IT WORKS!!

    image

    THEN I CONNECT THE DRIVER VCC TO POSITIVE 5V ON THE OUTPUT OF THE L7805 WITH AN ALLIGATOR CLIP. IT WORKS!!

     

    image

    OK! I WILL SOLDER THE DRIVER VCC TO THE OUTPUT OF THE L7805. IT DOESN'T WORK!! image

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to jehielmartinez

    I also just realized you seem to be using NMIH Rechargeable batteries, or a version of Rechargeable battery

     

    These are only 1.2V each and you appear to have only 4 in your holder, this adds up to 4.8V before the regulator, the reg also requires 2V more on the input to get the designated output (5V in this case). This would require nearer 7V from the batteries

     

    If you can simply try replacing the rechargeable with a fresh set of Alkaline to see if that is all it needs to make things work, re-routing the wire is also still a wise thing to do

     

    Do you have a meter to validate the voltage coming out of the regulator without the motor running and then with both motors on ?, if so what are the readings

     

    Regards

     

    peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to jehielmartinez

    I also just realized you seem to be using NMIH Rechargeable batteries, or a version of Rechargeable battery

     

    These are only 1.2V each and you appear to have only 4 in your holder, this adds up to 4.8V before the regulator, the reg also requires 2V more on the input to get the designated output (5V in this case). This would require nearer 7V from the batteries

     

    If you can simply try replacing the rechargeable with a fresh set of Alkaline to see if that is all it needs to make things work, re-routing the wire is also still a wise thing to do

     

    Do you have a meter to validate the voltage coming out of the regulator without the motor running and then with both motors on ?, if so what are the readings

     

    Regards

     

    peter