Arduino Forum Using LCD from LG nexus 4 and others on Arduino mega 2560
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
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 402 subscribers
  • Views 501 views
  • Users 0 members are here
  • smartphone
  • lcd
  • mipi
  • 2560
  • shield
  • arduino
Related

Using LCD from LG nexus 4 and others on Arduino mega 2560

matfur92
matfur92 over 11 years ago

Hi to all !!

Today I have a question:

Can I use LCD from old smartphones such as Nexus 4, G2 for example (view photos at the end of post) with my Arduino mega 2560?

I need of a particular shield? Does it exist? How it much?

Thanks a lot image

imageimageimageimageimage

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 11 years ago +1 suggested
    The only thing that comes close is this https://hackaday.io/project/364 , but I do not seem to be driven by arduino, but only a converter that uses Arduino as a component
Parents
  • Former Member
    0 Former Member over 11 years ago

    The only thing that comes close is this https://hackaday.io/project/364, but I do not seem to be driven by arduino, but only a converter that uses Arduino as a component image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • matfur92
    0 matfur92 over 11 years ago in reply to Former Member

    I think that you have reason...but it is a point of start image

    If it were possible to directly drive signals of HDMI would not hurt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • matfur92
    0 matfur92 over 11 years ago in reply to Former Member

    I think that you have reason...but it is a point of start image

    If it were possible to directly drive signals of HDMI would not hurt