Arduino
  • Products
  • More
Arduino
Arduino Forum Reverse Engineering old serial devices and cloning with arduino.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 416 subscribers
  • Views 1591 views
  • Users 0 members are here
Related

Reverse Engineering old serial devices and cloning with arduino.

e14 Contributor
e14 Contributor over 12 years ago

I guess this is a strange topic and might not be one anyone here could give any advice on but here goes...

 

I have a piece of music equipment that uses a remote control. This remote control communicates bi-directionally with the main unit.

It communicates over RS-422 protocol (mainly for the cable distance, i believe)

 

I have purchased a couple of rs422 to usb adaptors with the intention of snooping the data in both directions using some serial port monitoring software.

I havent quite gotten that to work properly on its own yet I think its most likely the connection settings I am attempting as the data I see looks messed up.

From what I can tell from the service manual this should be 8 Bit Characters with no parity and 2 stop bits.

 

Anyways, as this device is now archaic in terms of technology (1982, I believe) i think it would be a great candidate for cloning with an arduino.

 

The remote itself uses an old intel 8749 microcontroller. this was an MCS-48 based device (i think) which also had a small eprom built into it for program memory.

this was 8-bit with 3 I/O ports.

 

The remote unit basically has 12 old litronics DL-1414 alphanumeric 4 digit displays (which recieve an ascii character and hold it in their memory until refreshed), a bank of buttons and faders (which are conected via an adc) and a db level meter.

 

I have the service manual of the unit which goes into much more depth about the bit addressing scheme of the devices. Which I can upload.

 

I might be thinking about this the wrong way but my idea was to sniff and capture the data being sent and recieved to figure out what is sent, when for instance, a fader is moved. This I would imagine would then be easy to strap to a slide pot in arduino and then have that movement sent to the serial bus possibly with some control bits added and then the value.

 

I'd really appreciate some thoughts and maybe advice on how such reverse engineering can be tackled...

 

Thanks in advance,

Brad

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 12 years ago +1 suggested
    USB adapters aren't the best way to do this (but might be your only choice). A logic analyser or better still a scope and a logic analyser (built in or separate) are the ideal tools. You can use the scope…
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Also, forgot to mention, I also recorded the bi-directional data using both usb adaptors.

    That the host was sending on one and what the remote was sending on the other.
    In the screen shot attached, you can see that at idle, the remote (displayed in red) site there constantly spitting out <CC> while the host replies in BLUE (with 30 bytes??) with a repeating response until a parameter is changed.

    You can see from this where I got my results...

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    It looks as if you are on your way - if I were you the next thing I would do is to write my own program to run on MAC or PC to present and log the data (unless you can configure the terminal prog to do this). It would be much easier to understand if it's presented in packets the way the devices send it and then as you start to understand it you can add decoding features to your prog. I would would use the original Visual Basic (VB6) to do this but no doubt others would use something written in this century.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    Thanks MIchael,

    I'm also having a lot of fun trying to figure it out.

    I don't really posess the skills right now to go creating a program to 'present and log" the data.

    Would you mind ellaborating a little further on the purpose of this? If push came to shove, I'd employ the services of someone capable of doing this for me perhaps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    Thanks MIchael,

    I'm also having a lot of fun trying to figure it out.

    I don't really posess the skills right now to go creating a program to 'present and log" the data.

    Would you mind ellaborating a little further on the purpose of this? If push came to shove, I'd employ the services of someone capable of doing this for me perhaps.