Arduino
  • Products
  • More
Arduino
Arduino Forum can any body help me????
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 417 subscribers
  • Views 770 views
  • Users 0 members are here
Related

can any body help me????

e14 Contributor
e14 Contributor over 11 years ago

hey guys im here new to the family of the element14 and this is my first topic and i need your help with a small project im working on and my project is a motion detector with a GSM message alarm and i really have no idea about how to start this project and the only idea i have is starting with arduino uno and a laser and pir sensor but the problem is i dont know what is the right kit i must use and how to program the arduino to send an alert message from the GSM adapter to my cell phone so please please i need your help....

 

 

thank you so much,

 

your's Omar

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    HI there

     

     

     

    Whats the Laser for, the PIR will detect the movement and provide a simple input to any Arduino or Launchpad controller (They typically have an open collector output meaning it can pull a voltage down but not drive it up, a resistor to the + supply fixes that, when movement is detected it pulls the line to 0.

     

     

     

    A GSM shield will be required for calling the cell, im not sure in your area but this will possibly involve a monthly fee to connect to the phone system

     

     

     

    If the Arduino is going to be near a network connection it could be possible to send an SMS message without needing a GSM adapter, just a cheaper network shield

     

     

     

    What is your current skill level, I will provide some links for learning but I don’t want to scare you away so knowing your current skill will help to target you at the right stuff

     

     

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    actually im not very skilled because this is my first experience with the arduino and the main reason is that only a few people in iraq know about the arduino and the opened source micro controllers and this is my first project ever and why im using a laser because i was asked to use one so my idea is to use a red laser and a light sensor and im going to use a GSM just to make a prove of concept and probably in the future i will upgrade my project to a higher level by pairing two motion detectors in a network along with a one alarm system but all i need is to start for now image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    actually im not very skilled because this is my first experience with the arduino and the main reason is that only a few people in iraq know about the arduino and the opened source micro controllers and this is my first project ever and why im using a laser because i was asked to use one so my idea is to use a red laser and a light sensor and im going to use a GSM just to make a prove of concept and probably in the future i will upgrade my project to a higher level by pairing two motion detectors in a network along with a one alarm system but all i need is to start for now image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    OK, so like a line crossing sensor, break the beam and send an alarm to a cell phone... hmm let me think on that for a bit

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    eexactly peter thats what im trying to do.