Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Leonardo, why so unpoppular?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 419 subscribers
  • Views 795 views
  • Users 0 members are here
  • adoption
  • uno
  • leonardo
  • arduino
  • popularity
Related

Arduino Leonardo, why so unpoppular?

kidiccurus
kidiccurus over 11 years ago

I have been using the arduino leonard for quite a while and was wondering why it seems so unpopular compared to the uno online. It was released way back in July 2012 and yet still does not seen to be as popular as the uno. It is cheaper than the uno, has more more io and can emulate a keyboard and mouse, so why is it not more popular. I understand that it takes a while for new technology to be adopted but come on, it has been over a year. Why do you think no one uses it?

  • Sign in to reply
  • Cancel

Top Replies

  • bobcroft
    bobcroft over 11 years ago +1 suggested
    Samuel, I suspect it may be because there are so many cheap clone UNO boards out there. Additionally most libraries and code examples seem to be targeted at the UNO or predecessor. although the Leonardo…
  • bobcroft
    bobcroft over 11 years ago +1 suggested
    Samuel, in my earlier reply I did not intend to infer that the Raspi could emulate a mouse or keyboard but rather if a project required such inputs the Raspi might be a better choice. I can see how a friendly…
  • cncdan
    cncdan over 11 years ago +1
    I use a leo as a laser controller, I will be using one to drive a plotter soon and I will be using one to make a pendit for my cnc laser, router and plotter when it gets done. reasons cost, key board emulation…
Parents
  • bobcroft
    0 bobcroft over 11 years ago

    Samuel,

                   I suspect it may be because there are so many cheap clone UNO boards out there.  Additionally most libraries and code examples seem to be targeted at the UNO or predecessor.  although the Leonardo can emulate a mouse or keyboard, what practical use are these features?  If you needed such inputs then a Raspi might be a better choice.

    Who knows?  These are just my thoughts

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 11 years ago in reply to bobcroft

    I used the USB keyboard emulation to make a device to automaticly log me on to my schools computer system. It was mostly a tech demo, but it was a fun little project. I can see it being VERY useful for pranks (i.e. randomly moving the mouse and typing random letters). I don't think a raspi can emulate a keyboard and mouse. As for clone boards, come on China, let's see a nice cheap Leo clone.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kidiccurus
    0 kidiccurus over 11 years ago in reply to bobcroft

    I used the USB keyboard emulation to make a device to automaticly log me on to my schools computer system. It was mostly a tech demo, but it was a fun little project. I can see it being VERY useful for pranks (i.e. randomly moving the mouse and typing random letters). I don't think a raspi can emulate a keyboard and mouse. As for clone boards, come on China, let's see a nice cheap Leo clone.