Arduino
  • Products
  • More
Arduino
Arduino Forum Led help?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 418 subscribers
  • Views 596 views
  • Users 0 members are here
Related

Led help?

bradnorwood
bradnorwood over 11 years ago

I have a simple project I need help with. It's a dual 10 LED light which hangs from my glasses to light the area I'm working on. It's nothing major but, I'm good at 3d printing but know very little in electronics. They are 3 mm LED's 3.2 volts 20 ma. Can someone help me with wiring this to an easy battery pack that I can attached to my belt etc. It needs to power 20 of them and last for 2-4 hours maybe. thx!

  • Sign in to reply
  • Cancel

Top Replies

  • amgalbu
    amgalbu over 11 years ago +4
    I think the best solution is to make a parallel of two LEDs in series (see diagram) Each 150 ohm resistor dissipates 60 mW, so 1/4 W resistors are fine I assumed that 9V alkaline battery are going to be…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +2
    Hi Brad, you posted this in 3 different places, please remove two of them, nothing worse than having to answer the same thing 3 times or having threads going in different directions for the same thing…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to amgalbu +1
    The more in series the better and more efficient if your going to include a boost converter then perhaps 4 groups of 5 and about 18V supply don't forget though, if your using a LIPO, make sure its got…
Parents
  • amgalbu
    0 amgalbu over 11 years ago

    I think the best solution is to make a parallel of two LEDs in  series (see diagram)

    image

    Each 150 ohm resistor dissipates 60 mW, so 1/4 W resistors are fine

    I assumed that 9V alkaline battery are going to be used (mainyl because they are cheap and compact)

    The circuit draws current 200 mA. A 9V battery typically has a capacity of 400mAh so therically it would last 2 hours. You can wire two 9V batteries in parallel to extend this time

    Hope this helps!!

    Ambrogio

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to amgalbu

    I agree.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to amgalbu

    I agree.