Arduino Forum ESP8266 arduino wireless.
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
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 404 subscribers
  • Views 615 views
  • Users 0 members are here
  • controll
  • wireless
  • arduino
  • remote
Related

ESP8266 arduino wireless.

anej
anej over 11 years ago

Hello.

I am planning to build a remote controled car with 2 arduinos - one arduino for the car and one for the controller... Now i found this ESP8266 Serial WIFI Wireless Transceiver Modules and i don't know if this is a good thing to use with my project. Can i use two those modules for serial communication between two arduinos ??

 

  • Sign in to reply
  • Cancel

Top Replies

  • bobcroft
    bobcroft over 11 years ago +2 suggested
    Anej, As has been said the ESP8266 is a relatively new device and there is not a lot of information on its use yet. For your project I would use the CISECO wireless modules. CISECO do a wireless shield…
  • camuyano
    camuyano over 11 years ago +1 suggested
    Short answer yes with some notes: To use the ESP8266 you'll need to parse the strings you get from the device in order to get the data. The ESP will output different messages about status and things like…
  • scargill
    scargill over 11 years ago in reply to bobcroft +1
    I would tend to disagree - there is now a lot of information - there are several projects including the original ESPRESSIF AT code which now works as of the latest updates - the FRANKENSTEIN code and a…
Parents
  • camuyano
    0 camuyano over 11 years ago

    Short answer yes with some notes:
    To use the ESP8266 you'll need to parse the strings you get from the device in order to get the data. The ESP will output different messages about status and things like that that you'll need to handle. All data receive from the ESP will be on a line that starts with +IPD followed by message lenght then data terminated with carriage return line feed.

    With the ESP8266 you'll need an Access point or one of the them to be an access point. One of the module should be a server and the other a client. Then data can be sent from one to the other. This is a fairly new device, I think it supports direct Wifi but I have not use that.

     

    If you want a cleaner serial communication between two Arduinos and they are near one to the other, it may be easier to use a Bluetooth to UART module. Or if they are farther away an NRF24 wireless module is nice (range depends on environment), or maybe an Xbee (xbees tend to be more expensive). The bluetooth modules and the NRF25 are reasonably cheap. The NRF normally a little cheaper than the bluetooth.

     

    Do not get me wrong I am in love with the ESP8266 so I will encourage you to give it a try, it should work. You'll need some level shifting (a few resistor or else) to change 5v to 3.3v signals at least on the arduino TX signal (ESP's RX).
    This is just my opinion, I am no expert. Wait for others to reply before deciding.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • camuyano
    0 camuyano over 11 years ago

    Short answer yes with some notes:
    To use the ESP8266 you'll need to parse the strings you get from the device in order to get the data. The ESP will output different messages about status and things like that that you'll need to handle. All data receive from the ESP will be on a line that starts with +IPD followed by message lenght then data terminated with carriage return line feed.

    With the ESP8266 you'll need an Access point or one of the them to be an access point. One of the module should be a server and the other a client. Then data can be sent from one to the other. This is a fairly new device, I think it supports direct Wifi but I have not use that.

     

    If you want a cleaner serial communication between two Arduinos and they are near one to the other, it may be easier to use a Bluetooth to UART module. Or if they are farther away an NRF24 wireless module is nice (range depends on environment), or maybe an Xbee (xbees tend to be more expensive). The bluetooth modules and the NRF25 are reasonably cheap. The NRF normally a little cheaper than the bluetooth.

     

    Do not get me wrong I am in love with the ESP8266 so I will encourage you to give it a try, it should work. You'll need some level shifting (a few resistor or else) to change 5v to 3.3v signals at least on the arduino TX signal (ESP's RX).
    This is just my opinion, I am no expert. Wait for others to reply before deciding.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer