Arduino Forum ESP8266 arduino wireless.
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
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 404 subscribers
  • Views 616 views
  • Users 0 members are here
  • controll
  • wireless
  • arduino
  • remote
Related

ESP8266 arduino wireless.

anej
anej over 11 years ago

Hello.

I am planning to build a remote controled car with 2 arduinos - one arduino for the car and one for the controller... Now i found this ESP8266 Serial WIFI Wireless Transceiver Modules and i don't know if this is a good thing to use with my project. Can i use two those modules for serial communication between two arduinos ??

 

  • Sign in to reply
  • Cancel

Top Replies

  • bobcroft
    bobcroft over 11 years ago +2 suggested
    Anej, As has been said the ESP8266 is a relatively new device and there is not a lot of information on its use yet. For your project I would use the CISECO wireless modules. CISECO do a wireless shield…
  • camuyano
    camuyano over 11 years ago +1 suggested
    Short answer yes with some notes: To use the ESP8266 you'll need to parse the strings you get from the device in order to get the data. The ESP will output different messages about status and things like…
  • scargill
    scargill over 11 years ago in reply to bobcroft +1
    I would tend to disagree - there is now a lot of information - there are several projects including the original ESPRESSIF AT code which now works as of the latest updates - the FRANKENSTEIN code and a…
Parents
  • bobcroft
    0 bobcroft over 11 years ago

    Anej,

              As has been said the ESP8266 is a relatively new device and there is not a lot of information on its use yet.  For your project I would use the CISECO wireless modules. CISECO do a wireless shield that fits straight onto an UNO, MEGA or one of the clones.  These modules cost about £10 each in the UK.  They have very good range and are very easy to use, no level shifting is required because it is all built into the shield.  There is very good supporting documentation and code examples on the CISECO web site. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • bobcroft
    0 bobcroft over 11 years ago

    Anej,

              As has been said the ESP8266 is a relatively new device and there is not a lot of information on its use yet.  For your project I would use the CISECO wireless modules. CISECO do a wireless shield that fits straight onto an UNO, MEGA or one of the clones.  These modules cost about £10 each in the UK.  They have very good range and are very easy to use, no level shifting is required because it is all built into the shield.  There is very good supporting documentation and code examples on the CISECO web site. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • scargill
    0 scargill over 11 years ago in reply to bobcroft

    I would tend to disagree - there is now a lot of information - there are several projects including the original ESPRESSIF AT code which now works as of the latest updates - the FRANKENSTEIN code and a Lua interpreter (links here in various places) - sure they are works in progress but for example on the original Espressif code I now have a mobile App controlling several outputs and monitoring inputs and I can get it to work utterly reliably on both the AT command set and (if I don't get too ambitious) on the Lua interpreter - and as far as the latter is concerned the bugs are dying away by the day. There is even apparently an RTOS implementation coming along! £10 is too much unless you absolutely have to have WIFI - you can get an Ethernet card for half of that...  at £2.20 or so the ESP-01 is an unbelievable bargain and worth persevering with.  Links here if you're interested.  There's a fellow in here who has produced with Eagle an interface board that handles the level shifting and I'm doing my own. Armed with the EAGLE files anyone can get bare boards these days cheaply so I would imagine before long there will be a host of interfaces for the ESP-01 - worth sticking with if you're just experimenting right now.