Arduino Forum I am trying to figure out how to write a code that explains the queuing of a 2 way intersection with stop signs. Explain with leds who has the right away green means go red means wait
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
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 393 subscribers
  • Views 386 views
  • Users 0 members are here
Related

I am trying to figure out how to write a code that explains the queuing of a 2 way intersection with stop signs. Explain with leds who has the right away green means go red means wait

Former Member
Former Member over 10 years ago

Use ir sensors to detect an object which would be the car. So 2 sensors and 4leds

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to Former Member +1
    Fairly easy to use a simple state machine and a switch - case, if it where longer I would look at it differently but this is a pretty short and simple thing
Parents
  • D_Hersey
    0 D_Hersey over 10 years ago

    But if you wanted to put out a little more effort into it you could have car objects with member functions such as look_left(), look_right(), check_intersection().  Then you could set up the instantiations with their own theads.  You could then use tick-time to model slow-pokes and hotheads.  That would be interesting. . .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 10 years ago

    But if you wanted to put out a little more effort into it you could have car objects with member functions such as look_left(), look_right(), check_intersection().  Then you could set up the instantiations with their own theads.  You could then use tick-time to model slow-pokes and hotheads.  That would be interesting. . .