Arduino
  • Products
  • More
Arduino
Arduino Forum DC motor very slow discharge, mosfet to small ? 5v circuit.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 420 subscribers
  • Views 1342 views
  • Users 0 members are here
Related

DC motor very slow discharge, mosfet to small ? 5v circuit.

e14 Contributor
e14 Contributor over 11 years ago

Been playing around with a DC motor #learningByDoing

 

And found for some reason, my DC motor wont discharge at a normal rate/instant,

It's as if it keeps power, but it's slowing down, slower.. slower.. slower..  until it finally stops.

 

image

The motor is connected to the black/red wires to the left, and have a diode as fly back.

 

It's grounded through the P-fet in the top, via the red wire, and green to ground.

Yellow is the signal from the arduino on port A0,

 

See the video --

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

So what am i doing wrong here, since the charge is not instant?

 

any ideas ? image

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 11 years ago in reply to e14 Contributor +1
    Martin Just so we know there are no other issues, can you post the code. If you post the code, then highlight the code and click on the >> symbol , Syntax Highlighting and C++ it will insert it neatly…
  • jw0752
    jw0752 over 11 years ago in reply to mcb1 +1
    Hi Mark, This is very good information. I always wondered how code got posted so nicely. Thanks John
  • jw0752
    0 jw0752 over 11 years ago

    Hi Martin, I would put the motor and PFET on a seperate power supply and see what happens. Also you could look to see what is happening voltage wise or PWM at the gate of the PFET as this is what should control the motor speed. I do not know what your control circui or logic looks like so it is difficult to comment further. Interesting phenomenon and my curiousity is peaked. Look at your voltage changes preferably with a scope and trace back to the cause.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to jw0752

    After your suggestions i took the fet out of circuit measured it and testet it with a LED, checks out ok.

     

    Checked my voltages while "turning off" the DC.  and aparently it's the Arduino doing this.

    I was using digitalWrite on Analog 0, which usually works fine.

     

    But when measuring the voltage, aparently the voltage drops slowly as if it was a capacitor charging.

    anyway, change the code to analogWrite 0 and 255 for on and off, and now it turn on and off instantly as exspected. 

     

    Strange...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to e14 Contributor

    Hi Martin,  If Peter Oakes has a chance to look at this thread he will be able to tell us exactly what is going on.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    You say your using a PFET

     

    Is this a P Channel MOSFET or something else, can you please provide the part number

     

    The way you have everything connected as best I can see, the motor is on the high side of the supply and the FET is taking the black wire of the motor to ground based on the output of the Arduino, please confirm, provide a hand drawn schematic if needed to help

     

    If my assumption is correct then you have the wrong device

     

    PChannel fets need their gate taken to a negative value relative to the source and as this is connected through the motor to plus V, it should turn on but then once on it will sit at a floating voltage as now a current is passing through it, the source is no longet at +V, even when the gate goes back to +V, the back emf even with the diode still may be enough to sustain a small current (Heavy capacitive coupling between the pins of a fet), if you have a scope, you may see it oscillating

     

    If the PFET is connected to the high side of the power then you would need to pull the gate atleast 4V below the source to get it to turn on and even then only partly, this is the prefered configuration for a pchannel fet used as a switch, for low side, use an NChannel fet

     

    Hope this helps, if not, provide the schematic and a part number of the fet in use

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    your use of digital write 0 is correct, this should not be an issue

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to e14 Contributor

    Martin

    Just so we know there are no other issues, can you post the code.

    If you post the code, then highlight the code and click on the >> symbol , Syntax Highlighting and C++ it will insert it neatly, color it etc.

     

    image

    As Peter confirmed the Analogue I/O can be controlled digitally.

    You might want to confirm how you are powering this since you seem to have a display, and motor.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to mcb1

    Hi Mark,

    This is very good information. I always wondered how code got posted so nicely.

    Thanks John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to jw0752

    John

    Yes its a bit of a mystery isn't it.

    One thing to watch for is sometimes a space at the start will throw it off, and it thinks its an Excel spreadsheet.

     

    Sometimes I've had to edit it after its in the 'code' form to put lines back in.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 11 years ago

    Do you have a shutoff resistor between gate and source?  Can you post your schematic?