Arduino Forum DS1307 with seven segment display
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
  • State Not Answered
  • Replies 6 replies
  • Subscribers 403 subscribers
  • Views 839 views
  • Users 0 members are here
  • arduino
Related

DS1307 with seven segment display

Former Member
Former Member over 10 years ago

hello everyone,

Am a follower of Jeremy Blum tutorials and his book exploring arduino is the one assist me to know element14 arduino community.

 

my problem is how i can use DS1307 to track time for counting days and display it on seven segment display. i want counter to counting up days from 00 day to 99 days i.e counting up ( incrementing by one number) at the interval of 24hrs. However i manage to count with the use of  millis() but problem comes as i introduce RTC.....i want to use RTC for assisting counting number of days because millis() is messing on me once the arduino power is off.

i have

1. Arduino Uno

2. RTC-ds1307

3. crystal 32.768kHz

4. 2 pull up resistor each 2.2k

5. 2 Seven Segment Displays(Common Cathode)

6. 2 shift register, 74HC595

7. 16 resistor of 680Ohm for connection between shift registers and seven segment displays

 

 

i attachment of my diagram and arduino sketch for counting, anyone with the help in both diagram and arduino sketch i will appriciate.

 

[code]

#define LATCH 12

#define CLK 13

#define DATA 11

 

 

int i,j;

int digitOne[10] = {63,6,91,79,102,109,125,7,127,103};

int digitTwo[10]= {63,6,91,79,102,109,125,7,127,103};

 

 

//other stuff

unsigned long startTime;

 

 

void setup()

{

  startTime = now.unixtime();

  pinMode(LATCH, OUTPUT);

  pinMode(CLK, OUTPUT);

  pinMode(DATA, OUTPUT);

}

  void loop()

{

  int dayCount = (now.unixtime() - startTime)/ 86400;

  displayDaycount(dayCount);

}

displayDaycount(int numberOfDays)

{

  for(int i=0; i<10; i++){

    for(int j=0; j<10; j++){

      digitalWrite(LATCH, LOW);

      shiftOut(DATA, CLK, MSBFIRST, ~digitTwo[j]); // digitTwo

      shiftOut(DATA, CLK, MSBFIRST, ~digitOne[i]); // digitOne

      digitalWrite(LATCH, HIGH);

     

        }

  }

}

 

[/code]

 

here is my diagram:

 

image

  • Sign in to reply
  • Cancel
Parents
  • najath
    0 najath over 10 years ago

    see this nice tutorial on DS1307 and Arduino:

    https://learn.adafruit.com/ds1307-real-time-clock-breakout-board-kit

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to najath

    thanks najath for your quick reply, i had those tutorial from adafruits and they are very helpfull and its the one taking me this point

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • najath
    0 najath over 10 years ago in reply to Former Member

    so are you able to read/write to the RTC chip through I2C interface, and display data read from it on to seven segment display?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to najath

    Not real najath, i just got basic knowledge from adafruit. So now the issue is to use those ideas to implement in seven segment display

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • najath
    0 najath over 10 years ago in reply to Former Member

    can you a bit more specific on what is working for you and what is not?

    are you able to display numbers on the display?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • najath
    0 najath over 10 years ago in reply to Former Member

    can you a bit more specific on what is working for you and what is not?

    are you able to display numbers on the display?