Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum First project ever and need help!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 25 replies
  • Subscribers 416 subscribers
  • Views 2641 views
  • Users 0 members are here
  • help
  • first_project
  • ben_heck
  • question
Related

First project ever and need help!

e14 Contributor
e14 Contributor over 11 years ago

     To start i'm 15 and this is my first project that I have sat down and actually planned out. Also please note I have little to no programming skills. My plan is to build a vending machine that is powered by an arduino board. The arduino would power servo motors that would then dispense the item. My question is where do I even start. What kind of motors should I get? Can the arduino even run several motors? How can I make this connectable to an outlet? (not battery powered). What equipment do I need? I have so many questions I could write book. Any design tips and help I can get would be great. Also any design changes you think would make the idea more efficient do share.Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 11 years ago in reply to e14 Contributor +1
    A good way to do this would be to use a DC motor that will rotate at a fixed speed. You can then control that using your arduino while timing a 360 operation and/or using a optical sensor to detect a complete…
  • gadget.iom
    gadget.iom over 11 years ago in reply to gadget.iom +1
    As this post looks like it is going to be mostly Arduino based you may want to move this post to The specified item was not found. . You can do this by clicking 'Move' in the menu on the right.
Parents
  • gadget.iom
    0 gadget.iom over 11 years ago

    Hi Chris

     

    That's a very ambitious first project. Your best approach it to break the whole thing down into a series of smaller tasks.

    You mention servo motors, a good arduino article about them can be found here; Arduino - Sweep

    What are you looking to dispense with this machine? How do you envisage servo's achieving the vending operation?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to gadget.iom

    Thanks for the reply my original idea was to use servos to rotate a large coil that would then drop the item, but thinking about it a servo wouldn't work a would need a whole motor to rotate the coil to be ready to dispense again and servo would just rewind back to its previous state. Except I have no experience with the code. Would it be fairly difficult to make a code that rotates the motor enough to make only one item dispense? and also have a delay so it can't be spammed?

     

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to gadget.iom

    Awesome that's one problem down another problem I thought about was how could I make it so that a certain button powered a certain motor? and could a arduino power more that 3-4 motors?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to gadget.iom

    So if (for example) your motor takes 5 seconds to complete a full revolution the Arduino could actuate the motor for a second or two, then wait for the photo-sensor to activate upon the full revolution. The Arduino can continue timing the revolution and If the interruption does not occur within 6 or 8 seconds the motor will stop and that vending slot will be disabled.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    You could use shift registers to increase the number of inputs/outputs, but for the sake of simplicity you may want to look at the Arduino Mega which will increase the available digital I/O to 54.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to gadget.iom

    How does the wiring for something like this work? Could I use a breadboard?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    You can indeed. Use some male-male jumper wires to link Arduino pins to the breadboard.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to gadget.iom

    As this post looks like it is going to be mostly Arduino based you may want to move this post to The specified item was not found.. You can do this by clicking 'Move' in the menu on the right.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to gadget.iom

    For supplies would I need stuff like voltage regulators and transistors or no?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    Voltage regulators possibly, depending on the supply voltage and the voltage of your peripheral components (motors etc). Transistors, almost certainly. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to gadget.iom

    So from my understanding so far when I click the button it will be hooked up to the arudino which will then tell a dc motor to spin a full 360 degrees then stop?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    Put simply... yes image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    Put simply... yes image