Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino is freaking out.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 417 subscribers
  • Views 563 views
  • Users 0 members are here
  • problem
  • com
  • help
  • hardware
  • code
  • uno
  • arduino
Related

Arduino is freaking out.

e14 Contributor
e14 Contributor over 11 years ago

I am making a moving turret on my Arduino uno and programming it.  But when I upload my code, the arduino restarts  like 15 seconds before the IDE says done uploading. Also, it takes a minute to upload no matter what code I use.(Even if I use the bare minimum example.)  When it does say done uploading it also has this message "  avrdude: stk500_getsync(): not in sync: resp=0x00   ."  The arduino also just lights up one of my leds when I have told it not to. I even uploaded the basic blinking code for the built-in led on pin 13 to see if it was my code, but it didn't change a thing.  I checked the COM ports and  made sure I selected the arduino uno. Is there a fix for this? And is it me or my arduino or my computer or etc.?

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    It looks like your Arduino may not be programmed with a boot loader or the serial interface is damaged somehow I am assuming the Arduino does not complete loading or even starts loading there are switches…
Parents
  • gadget.iom
    0 gadget.iom over 11 years ago

    Are you using pins 0 and 1 on your UNO?

     

    If so, there may be some conflict as these pins are shared with the serial connection used to upload the sketch.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to gadget.iom

    Thanks, Paul, that fixed the problem. But do you know if I can still use those pins after I upload the sketch?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    Hi Kyle

     

    Yes you can reconnect the pins and they will function. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    Hi Kyle

     

    Yes you can reconnect the pins and they will function. image