Arduino Forum Quadcopter help
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
  • State Not Answered
  • Replies 5 replies
  • Subscribers 393 subscribers
  • Views 456 views
  • Users 0 members are here
Related

Quadcopter help

Former Member
Former Member over 10 years ago

I'm planning on building a quadcopter using an arduino. I want a live feed FPV camera and a few other angles,. Is it possible to use an arduino or a raspberry PI for that? I would prefer delay of less than 1second, perferably instant.

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago in reply to clem57 +1
    Take a look at this idea! @ http://www.element14.com/community/roadTestReviews/1863 ...
  • ipv1
    0 ipv1 over 10 years ago

    You can use raspberry pi. Google gstreamer and you should get there... image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago

    @Michael Cassara ,

     

         Question: Are you using camera for guidance of the quadcopter? If not, @Inderpreet Singh has the easiest solution. Otherwise I would go for the arduino only if you have enough memory for controlling quadcopter as well as the FPV camera. This really turns out to be resources of the processor/memory. Please specify which Arduino or clone you are looking at.

     

    Thanks,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    I'm planning of using it to control the quadcopter, I want to be able to fly it outside while I'm inside using a x52 controller preferably so if I can get the arduino to communicate via bluetooth, wifi, internet or somthing with my computer that would be nice, I'm gunna try to use the uno but I may need the mega.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    Check out this http://hackaday.com/2015/01/26/using-rc-transmitters-with-flight-simulators/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to clem57

    Take a look at this idea! @http://www.element14.com/community/roadTestReviews/1863...